成功案例

Transmission manufacturer relies on LMS Engineering to strengthen its position as technology partner with automotive OEMs

Aisin AW

Aisin AW reduces booming, judder and gear noise, and implements best-practice NVH techniques across its standard development process

Tackling new vibrations

In the automotive industry, the pursuit for greater efficiency, lower emissions and a “greener” brand image has put pressure on subsystem and component design. While dealing with a downsized engine, transmissions should operate as effectively as possible with a minimum of losses. To optimize performance and minimize losses, the torque converter should be used as little as possible, resulting in early engagement of the lock-up clutch. Trends for producing higher torque at lower engine revolutions per minute (RPMs), together with an earlier clutch lock-up required for efficiency savings, have increased the propensity for vibrations and thus can create comfort and durability issues.

A 10-year partnership

As the world’s largest automatic transmission manufacturer (market share), Aisin AW is continuously seeking operational improvement. One especially productive venture occurred in 2003, when the company put together a team of subject matter experts to find solutions for future quality issues. The experts examined, for example, how to deal with gear whine and how to cope with the torque converter. Looking for a technology partner, Aisin AW engaged the LMS™ Engineering services of product lifecycle management (PLM) specialist Siemens PLM Software to solve a gear whine issue.

Before Aisin AW collaborated with LMS Engineering experts, the company worked in a troubleshooting mode for solving noise, vibration and harshness (NVH) issues. “At that time, 20 percent of the gearboxes had noise issues,” explains Hiroki Tsuji, group manager of the starting device analysis group, core Component Engineering Aisin AW. “LMS Engineering recommended a transfer path analysis (TPA) and helped with a combined simulation and test approach to understand the relation between noise sources, vibration and the effect on perceived user comfort.”

One year later, Aisin AW and LMS Engineering signed a framework agreement, which was expanded in 2006 to fulltime, on-site assistance by an LMS expert. The on-site assistance engendered close collaboration and helped Aisin AW solve durability and NVH issues, including gear whine, gear rattle, booming, torsional vibrations and transient phenomena such as judder and shift shock. LMS experts used advanced methodologies, including testing solutions and 3D to 1D model-based system engineering (MBSE) solutions.

“Thanks to technology transfer between the companies, Aisin AW now addresses issues such as gear whine and judder upfront in the design phase,” says Tsuji. “Many NVH techniques we learned from LMS Engineering are now part of our standard development process, such as transfer path analysis.”

Eliminating clutch judder

“In one of our recent projects with LMS Engineering, we wanted a full vehicle, model based approach for the prediction and elimination of clutch judder,” says Tsuji. The cause of self-excited clutch judder is known to be the lock-up clutch friction characteristics. It was important for Aisin AW to understand if and when this phenomenon would occur in any given application. “Additionally, we were seeking to evaluate transmissions at an early stage to reduce the chances of self-excited judder occurring when prototypes are built,” Tsuji continues.

LMS Engineering applied a customized powertrain NVH solution, using LMS Imagine.Lab™ software, and correlated the simulation models with the test bench data. “Based on LMS 1D simulation tools, we identified the root causes,” says Tsuji. “Our engineering team can now make correct design choices during the concept phase and support troubleshooting if judder arises at the prototype stage. When making the prototype afterwards, we are certain it is judder-free.”

Reducing low-frequency booming

In another project, Aisin AW contacted LMS Engineering to help them solve a low-frequency booming noise issue. Low frequency booming is a relatively new phenomenon and a consequence of engine downsizing and restrictions on torque converter usage. Fewer cylinders mean that more torque is transferred per cylinder, which results in higher forces that are less balanced and damped within the transmission.

As the appearance and severity of the booming vibration issues depend on the combination of the vehicle body, suspension, transmission and damper, Aisin AW wanted to gain insights into the root causes at each level, and learn how to create a model that could accurately reproduce the phenomena. LMS Engineering experts developed a full vehicle modeling approach combining test-based description of the vehicle body, 3D suspension modeling in LMS Virtual.Lab™ Motion software and 1D powertrain modeling in LMS Imagine.Lab Amesim™ software.

“The results of the full vehicle simulation gave us very good insight into the root causes of the booming noise at each level,” says Tsuji. “By changing the design, we could drastically reduce the booming peak.” The overall result was very effective, and Aisin AW has included the 1D simulation software and the test technology in the development program.

Preferred partner for automotive OEMs

The long-term relationship between the technical experts of Aisin AW and LMS Engineering is based on two common aspects of each company’s identity: high quality standards and innovative technology. The unique combination of test and simulation techniques and troubleshooting capabilities of LMS Engineering services helped Aisin AW to maintain its image as an innovative technology leader. “Applying LMS Engineering troubleshooting techniques, we realized about a 50 percent time reduction to come to a solution,” explains Tsuji.

Today, Aisin AW works in close collaboration with automotive OEMs to optimize fuel consumption via an integrated approach. The company continuously seeks find a more global solution to answer current and future challenges. Tsuji notes, “The 10-year partnership with LMS Engineering significantly strengthened our position with automotive OEMs. Automakers now recognize Aisin AW as a valuable technology partner. Together, we work towards improved fuel consumption while ensuring comfortable driving.”

Close share layer

Share this page

Share this page through any of the following channels.

Bookmarking Sites

Communities

News

Blogs & Microblogs