新闻发布

中国,北京, September 6, 2017

西门子与惠普携手推动3D打印在产品开发和工业生产中的应用


  • 惠普的Multi Jet Fusion 3D打印技术与Siemens PLM Software的旗舰软件NX集成,用于产品开发和制造
  • 专为惠普Multi Jet Fusion开发的西门子NX增材制造软件模块已经正式通过惠普认证以用于生产级工业3D打印 
  • 双方深化合作伙伴关系,为下一代惠普Multi Jet Fusion 3D打印机制定技术路线图

在长期合作关系的基础上,Siemens PLM Software开发的增材制造(AM)模块已获得惠普公司的认证,该模块将会加速3D打印在生产过程中的应用。用于HP Multi Jet Fusion的Siemens NX AM这一全新的软件模块将把Siemens PLM Software的“端到端”、从设计到生产的解决方案扩充至增材制造领域。NX™软件模块使客户能够在单一软件环境中为其惠普3D打印项目开发和管理零部件,避免昂贵耗时的数据转换过程,以及第三方工具,从而提高从设计到成品的整体工作效率。西门子和惠普也在调整未来技术路线图,使设计人员和工程师能够重新构思设计产品,充分利用惠普的3D打印能力,避免传统制造的限制,以更快的速度和更好的成本效益生产新产品,从而为工业3D打印在创新设计领域的应用提供显著的机会。

西门子的新软件模块使NX客户能够用极少的步骤将惠普Multi Jet Fusion 3D打印零件的设计、优化、仿真和打印任务的准备,以及检验过程集成到一个受控环境中。用户现在可以将多个3D零件模型加载到NX中,自动组合嵌套并将其提交给惠普3D打印机,所有这些工作将全部集成在一个统一环境中,以极少的步骤就可完成。在未来,通过NX和Multi Jet Fusion集成,软件应用或工序之间不再需要数据转换,从材料特性到独立体素层面实现前所未有的控制水平。这将实现对不同的材质、密度、强度和摩擦系数以及热、电和传导特性零件的3D打印。

惠普公司3D打印商业拓展及开发全球负责人Michelle Bockman表示:“惠普和西门子将最优秀的设计和制造工作流程软件进行集成,以实现最佳的3D打印,为制造在速度、质量和经济性上满足当今数字化工业时代要求的新产品创造可能。我们期待与西门子加强合作,通过Multi Jet Fusion 3D打印解决方案的体素级设计能力,不断满足客户日益提高的需求。”

西门子和HP有一个共同目标,那就是增材制造产业化。备受赞誉的惠普Multi Jet Fusion 3D打印解决方案是可以直接用于生产的商用系统,在打印高精度1 零件时,能够以当前3D打印系统10倍2的速度和一半3 的成本完成打印。通过将Siemens PLM Software的涵盖产品生命周期管理(PLM)和电子设计自动化(EDA)软件、集成自动化与制造作业管理的完整解决方案与惠普的3D打印解决方案结合,增材制造能够成为一个真正的工业生产过程。两家公司将继续协作,同时联合其它行业领导者,共同打造一个重要的合作伙伴生态系统,最终实现使增材制造成为一种工业化生产方法的愿景。

Siemens PLM Software制造工程软件业务高级副总裁Zvi Feuer指出:“西门子视增材制造为变革性的数字力量,它促使公司重新设计其工厂和产品以提升业绩水平。由于现代企业愈发期望加快产品上市速度、差异化产品性能、简化生产及供应链作业并实施新的业务模式,对于西门子来说,加深与惠普之间的伙伴关系并推动惠普的创新型3D打印技术变得尤为关键。随着产品不断复杂化和个性化,我们期待由多种材料构成、可调机械性能和集成电子的下一代3D打印零件的诞生。”

若要了解更多信息,请见: (西门子的增材制造产业化之路:转变观念,步步为营).

  1. 基于喷砂试验后的尺寸精度不低于±0.2毫米/0.008英寸。见 hp.com/go/3Dmaterials,更详细地了解材料规格参见hp.com/go/3Dmaterials。基于下列机械属性:抗拉强度为50,系数Z为1900,系数XY为1900。用PA-12材料进行ASTM标准测试。
  2. 内部测试及仿真结果显示,HP Jet Fusion 3D打印解决方案的平均打印速度比2016年4月市面上出售的价格区间为10万美元至30万美元的FDM和SLS打印机快10倍。测试变量:零件数量 -堆积密度为在上述竞品仪器的相同数量零件的20%的HP Jet Fusion 3D打印零件1满桶;零件重量:30克;层厚:0.1毫米/0.004英寸。通过2017年推出的具有快速冷却功能的惠普Jet Fusion 3D加工站进行快速冷却。与价格区间在10万美元到30万美元的SLS打印机解决方案的推荐制造时间(2016年4月测试结果)相比,具有快速冷却功能的惠普Jet Fusion 3D加工站缩短了零件冷却时间。FDM不适用。
  3. 内部测试及公开数据显示,惠普Jet Fusion 3D打印解决方案的平均单位零件打印成本仅为2016年4月市面上出售的价格区间在10万美元到30万美元的具备可比性的FDM和SLS打印解决方案的一半。成本分析依据:制造商推荐的标准解决方案配置价格、物资价格以及维护成本。成本标准:用制造商推荐的粉末可重用性比例,以10%的堆积密度打印重30克的零件,一周打印5天,每天打印1到2桶。

Siemens PLM Software ,Siemens PLM Software是全球领先的产品生命周期管理(PLM)和制造运营管理(MOM)软件、系统与服务提供商,拥有超过1,500万套已发售软件,全球客户数量达140,000多家。公司总部位于美国德克萨斯州普莱诺市。Siemens PLM Software与企业客户充分合作,为其提供领先的行业软件解决方案,帮助其通过革命性创新获得可持续性竞争优势。欲详细了解Siemens PLM Software的产品和服务,敬请访问: www.siemens.com.cn/plm .

敬请关注西门子中国官方微博http://weibo.com/siemens 和西门子媒体微信公众账号“西闻联播”(微信号xiwenlianbo)。 如需了解西门子的更多创新故事,请关注《未来之窗》:www.siemens.com.cn/pof

Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world’s largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.

HP Inc. creates technology that makes life better for everyone, everywhere. Through our portfolio of printers, PCs, mobile devices, solutions and services, we engineer experiences that amaze. More information More information about HP Inc. is available at http://www.hp.com .

Note: Siemens and the Siemens logo are trademarks or registered trademarks of Siemens AG. NX is a trademark or registered trademark of Siemens Product Lifecycle Management Software Inc. or its subsidiaries in the United States and in other countries. All other trademarks, registered trademarks or service marks belong to their respective holders.

Primary Contact

李 曦
+86-10-8520 3952
li.xi@siemens.com

Close share layer

Share this page

Share this page through any of the following channels.

Bookmarking Sites

Communities

News

Blogs & Microblogs