中国,北京, 29 October 2015

西门子在Rescale的按需云平台上扩展其NX仿真解决方案

西门子近日宣布,用户现在可通过Rescale提供的动态可扩展型按需云仿真及高性能计算(HPC)平台获取其综合性NX™ 软件组合中的热分析和流体分析仿真解决方案。由于西门子的NX™ Nastran® 软件此前已经能在Rescale上进行部署,此次的功能扩展将在全球最大的HPC硬件网络上为客户提供更加广泛的西门子仿真产品选择。Rescale仿真平台可无缝集成定制化的HPC基础架构与仿真软件,并使用户可以直接通过网页浏览器获取这些资源。该平台可以帮助工程师和科研人员缩短产品开发时间,进而提高效率、推动创新、改进产品质量并加快上市速度。

制造业正面临一个共同的趋势:仿真的模型对象越来越庞大复杂,企业需要通过模拟仿真来探索更多的设计选项,并对包括结构、热学和流体特性等多物理学科领域进行仿真。通过Rescale平台访问西门子的解算器以解决来自不同学科领域的问题,能帮助各种规模的企业实现灵活的HPC投资。通过这一解决方案,工程师可以轻松开展试验设计(DOE)、多学科设计探索以及独立或多解算器仿真,实现具有成本效益的大型仿真,从而对设计选项进行更彻底的评估。

Siemens PLM Software产品工程软件高级副总裁Jim Rusk 表示:“我们很高兴加入NX Flow 和NX Thermal解算器,以进一步扩大Rescale仿真平台上的仿真工具组合。客户越来越倾向于选择更加灵活的、可扩展的高性能计算方式,而Rescale通过其全球网络所提供的强大安全的在线服务,将助力增强我们的核心仿真产品的领先优势。”

工程师可以通过软件许可证或利用Rescale提供的“按使用计费”的许可证,来使用Rescale云环境中的NX解算器。“按使用计费”的方法极其灵活,可以满足用户不同的计算需求。客户还能享受预付款折扣优惠,获得更高的价值。

Rescale 首席执行官Joris Poort认为:“Rescale高度重视与Siemens PLM Software保持紧密的合作伙伴关系。我们很高兴能进一步扩展Rescale平台上的西门子仿真工具,为双方共同的客户提供更好的服务。在从传统的本地部署向灵活的HPC云平台及按需部署的巨大转变过程中,通过以灵活的按时计费模型提供NX解算器组合, Siemens PLM Software进一步加强了其在仿真领域的技术和思想领袖地位。”

如欲详细了解西门子与Rescale的合作伙伴关系及其对仿真领域的贡献,用户可于2015年10月28日星期三上午8:00时(太平洋夏令时间)/上午11:00时(东部夏令时间),参加 “通过Rescale 云平台上的NX Thermal/Flow加快工程设计过程网络研讨会(英文)”。届时现场模拟演示NX Thermal/FlowRescale在云仿真平台上运行时的强大功能和易用性。此外,热-流体系统的参数研究和DOE分析也将是此次研讨会的重点。用户可登录https://attendee.gotowebinar.com/register/2038424558773177345进行注册。

欲了解NX Flow和NX Thermal的更多信息,请访问网站:www.siemens.com/plm/nxcae

西门子数字化工厂集团旗下机构Siemens PLM Software是全球领先的产品生命周期管理(PLM)和生产运营管理(MOM)软件、系统与服务提供商,拥有900万套已发售软件,全球客户数量达77000家。公司总部位于美国德克萨斯州普莱诺市。Siemens PLM Software与企业客户充分合作,为其提供领先的行业软件解决方案,帮助其通过革命性创新获得可持续性竞争优势。欲详细了解Siemens PLM Software的产品和服务,敬请访问:www.siemens.com/plm.

如需了解更多信息,请访问西门子中国网站:www.siemens.com.cn/plm。 敬请关注西门子中国官方微博http://weibo.com/siemens和西门子媒体微信公众账号“西闻联播”(微信号xiwenlianbo)。

About Rescale

Rescale’s simulation platforms are the leading global solutions for the secure deployment of simulation software and high performance computing (HPC) hardware in the enterprise. Rescale partners with industry-leading software vendors to provide instant access to a variety of simulation packages while simultaneously offering customizable HPC hardware. Headquartered in San Francisco, CA, Rescale’s customers include global Fortune 500 companies in the aerospace, automotive, life science, and energy sectors. For more information on Rescale products and services, visit www.rescale.com.

Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world’s largest producers of energy-efficient, resource-saving technologies, Siemens is No. 1 in offshore wind turbine construction, a leading supplier of combined cycle turbines for power generation, a major provider of power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2014, which ended on September 30, 2014, Siemens generated revenue from continuing operations of €71.9 billion and net income of €5.5 billion. At the end of September 2014, the company had around 343,000 employees worldwide on a continuing basis. Further information is available on the Internet at www.siemens.com.

Note: Siemens and the Siemens logo are registered trademarks of Siemens AG. NX is a trademark or registered trademark of Siemens Product Lifecycle Management Software Inc. or its subsidiaries in the United States and in other countries. NASTRAN is a registered trademark of the National Aeronautics and Space Administration. Rescale and the Rescale logo are registered trademarks of Rescale, Inc. All other trademarks, registered trademarks or service marks belong to their respective holders.