中国,北京, 14 July 2015

西门子最新版Solid Edge软件帮助工程师加速产品设计,提高设计灵活性

最新版本的西门子Solid Edge® 软件 (Solid Edge ST8) 的增强版功能和新功能,可以帮助用户提高设计速度,增强其利用同步建模技术的能力,并在平台和购买选项方面为用户带来更大的灵活性。除此以外,运行微软Windows 8.1操作系统的平板电脑现已可以安装完整版Solid Edge ST8,进一步扩大了用户随时随地进行设计的自由。除了发布Solid Edge ST8之外,西门子的产品生命周期管理(PLM)业务同时还发布了一款新的移动应用Solid Edge App Marketplace℠ mobile app Marketplacesm。这是为附加解决方案而设计的一站式购买商店,旨在拓展Solid Edge的功能,帮助客户进一步提升其产品开发效率。

Kimball International研发工程经理Ricardo Espinosa表示:“我非常满意Solid Edge ST8中对同步建模技术界面所做的功能提升。这些增强版功能可以加快学习速度,帮助我们更好地培训实习生和临时工,让他们可以尽快跟上工作节奏。很明显,Solid Edge开发团队一心为客户创造价值,并致力于提供先进的产品开发工具。”

同步设计意图管理、复杂草图绘制以及3D特征识别等功能的增强,可以帮助用户专注于设计任务本身,而不是设计工具,从而加速建模过程。灵活的建模方式结合同步建模技术,为用户提供了更大的自由度,使其能够以直观的方式更快地交付精确逼真的设计,缩短上市时间。同步建模技术不仅拥有对尺寸驱同步建模技术不仅拥有对尺寸驱动设计的精确控制,同时还结合了直接建模的速度和灵活性。

此外,Solid Edge ST8简化了处理大型复杂装配体的功能,结合其精确仿真和预测运动学条件的能力,不仅大幅加速了装配体设计流程,同时也显著减少了对实物模型的需求。Solid Edge ST8还拓展了内置学习工具、网络社区及新Solid Edge App Marketplace的访问权限。这些工具和产品特征具有一个共同的设计意图,就是通过加快设计流程,提高绩效和生产效率。购买选项的多可选性,包括按月租用,旨在满足不同的业务需求,使客户可以根据自身财务状况灵活地选择。

Solid Edge ST8还提供完全支持Windows 8.1多点触控体验的界面,并且能够区别手指和触笔的不同,使用户可以以更加直观的方式进行设计。通过移动平台全面访问设计流程的功能,不仅实现了地理位置上的灵活性,而且更有利于创新和协同。

Lifecycle Insights研究分析师Chad Jackson认为:“与那些已经在平板电脑上使用Solid Edge进行设计的用户交流后,我发现西门子并不只是简单地建个端口而已。实际上,西门子对于如何使Solid Edge适应移动环境以便充分利用多点触控和触笔交互的优势是经过深思熟虑的。经过交谈,我发现无论用户身在何处,这些应用程序都能帮助他们与供应商实现协作并持续解决客户需求,为他们创造真正的价值,而这也正是现代工程师所需要的。”

Siemens PLM Software主流工程软件高级副总裁John Miller指出:“Solid Edge ST8显著增强了可访问性和易用性。我们相信,对客户而言,拥有如何购买和部署Solid Edge的自由是非常重要的。无论他们选择的是永久许可还是月租许可,是台式工作站还是全面移动平台,我们都能为各种规模的企业提供满足其业务需求的适当解决方案,以帮助Solid Edge的客户实现更好的设计和创新。”

Solid Edge ST8计划今年夏天发售。欲了解更多信息,敬请访问www.siemens.com/plm/st8.

西门子数字化工厂集团旗下机构Siemens PLM Software是全球领先的产品生命周期管理(PLM)和生产运营管理(MOM)软件、系统与服务提供商,拥有900万套已发售软件,全球客户数量达77000家。公司总部位于美国德克萨斯州普莱诺市。Siemens PLM Software与企业客户充分合作,为其提供领先的行业软件解决方案,帮助其通过革命性创新获得可持续性竞争优势。欲详细了解Siemens PLM Software的产品和服务,敬请访问:www.siemens.com/plm.

Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world’s largest producers of energy-efficient, resource-saving technologies, Siemens is No. 1 in offshore wind turbine construction, a leading supplier of combined cycle turbines for power generation, a major provider of power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2014, which ended on September 30, 2014, Siemens generated revenue from continuing operations of €71.9 billion and net income of €5.5 billion. At the end of September 2014, the company had around 357,000 employees worldwide. Further information is available on the Internet at www.siemens.com.

Note: Siemens and the Siemens logo are registered trademarks of Siemens AG. Solid Edge is a trademark or registered trademark of Siemens Product Lifecycle Management Software Inc. or its subsidiaries in the United States and in other countries. Windows is a registered trademark of Microsoft Corporation. All other trademarks, registered trademarks or service marks belong to their respective holders.

主要联系方式


+86-10-8520 3952
li.xi@siemens.com