Smart product and process design for consumer goods

A collection of smart products designed using the power of the digital twin.

Consumer goods manufacturing is a dynamic industry that requires companies to keep up with ever-changing trends. As consumers become increasingly conscientious about the products they purchase and the types of companies they buy from, consumer goods manufacturers discover that they must adapt their products faster than previously anticipated. Additionally, customers want unique product experiences and instant access to advanced, connected devices and commodities. To deliver exceptional customer experiences, consumer product manufacturers must develop new behaviorally responsive products that meet sustainability standards while improving consumers' lives.

Implementing a plan based on a digital thread validation strategy can aid manufacturers in overcoming some of their most significant challenges. Smart product design and process design enable companies to leverage simulation and concurrent production to ensure manufacturability at the required speed, quality, and cost as an integrated total product solution.

Consumer goods manufacturing is a dynamic industry that requires companies to keep up with ever-changing trends. As consumers become increasingly conscientious about the products they purchase and the types of companies they buy from, consumer goods manufacturers discover that they must adapt their products faster than previously anticipated. Additionally, customers want unique product experiences and instant access to advanced, connected devices and commodities. To deliver exceptional customer experiences, consumer product manufacturers must develop new behaviorally responsive products that meet sustainability standards while improving consumers' lives.

Implementing a plan based on a digital thread validation strategy can aid manufacturers in overcoming some of their most significant challenges. Smart product design and process design enable companies to leverage simulation and concurrent production to ensure manufacturability at the required speed, quality, and cost as an integrated total product solution.

A commercial expresso maker. A smart product designed using the power of the digital twin.

Learn More

Given the concerns confronting consumer goods manufacturers today, having access to an integrated end-to-end product development portfolio that enables digitalization is critical. Combining a multi-disciplinary approach to development and virtual validation with simulation and concurrent smart product design solutions ensures manufacturability at the desired speed, quality, and cost.

The digital twin's power enables manufacturers to develop products responsive to consumers' needs and desires, bridging the gap between concept, design, and production.

Discover the power of the digital twin

Multi-disciplinary product design includes digital twin products, and digital twin manufacturing. As a complete set of solutions, manufacturers can use it to virtually design any smart product and connect it to its manufacturing process, building an integrated environment while considering all change drivers.

Process design and validation let companies implement parallel development processes while maximizing design reuse and increasing collaboration by connecting processes and a single data source for materials, geometry, electronics, software, packaging, artwork, tests, and production data.

Manufacturing validation enables manufacturers to determine whether products can be manufactured and packaged virtually. This process allows for the elimination of physical testing and reduced production time. Additionally, manufacturers can run hundreds of iterations to optimize the design of their product and manufacturing process for quality, cost, and manufacturability.

Explore smart product and process design

By utilizing cutting-edge technologies, consumer goods manufacturers can reap the benefits of product and manufacturing simulation processes such as design automation, design optimization, and virtual validation. Having access to innovative solutions ensures that brands can effectively launch new smart products and modify current ones. These technological capabilities will allow all brands to keep up with existing trends and be abreast of emerging concepts while remaining relevant.

Click to explore more about our solutions for product design and validation and process design and validation.

A commercial expresso maker. A smart product designed using the power of the digital twin.

解决方案功能

Explore the key areas of this solution.

Design for Additive Manufacture

增材制造正在实现以前不可能实现或过于昂贵而无法实现的优化设计,从而改变产品的设计方式和制造方式。 使用全新的增材制造方法设计、优化和构建金属和塑料组件。

Environmental Compliance & Product Sustainability

保持合规并满足您的如下可持续性需求:材料和物质管理、自动化供应商申报处理、环境符合性评级和报告,以及可持续发展的 PLM 框架产品。

Fluid dynamics simulation

Simcenter 提供了业界前沿的计算流体动力学软件,让您得以对任何包含液体流或气体流(或两者的组合)和所有关联物理场的工程问题进行模拟。

Industrial Design & Styling

独特的设计和造型增加了企业的竞争优势。 我们的产品可提供灵活、可靠的计算机辅助工业设计和造型软件,通过提供可直接用于建模的快速概念设计,加速您的产品工程设计。

Manufacturing Process Planning

高效编写制造流程计划,并将其有效地传递和扩展到整个企业当中。

Structural simulation

不论所处行业为何,了解组件或产品装配体在应力或振动条件下如何反应都至关重要;面对越来越复杂的产品和材料,除了线性静力学分析,工程师还需要其他工具。Simcenter 将解决广泛的结构分析问题所需的解决方案集成到一个单一的用户环境中。

适应性强的 PLM 基础

适应性较强的产品生命周期管理 (PLM) 系统可以帮助您快速应对业务或市场巨大冲击带来的变化。由于 PLM 可以通过 Web 浏览器、所有设备以及人们日常使用的设计工具和办公应用程序访问,因此在企业范围内开展协同将变得异常简单。您可以从灵活的部署方案(内部部署、云和 SaaS)中进行选择,从而缩短价值实现时间并降低拥有成本。

对 [[global-preference-center-interest-placeholder]] 感兴趣?

订阅 [[global-preference-center-interest-placeholder]] 更新信息

哦!

抱歉,我们无法捕获您提交的信息。请重新尝试。

感谢注册!首次订阅?确保选中电子邮件以确认订阅。

字段为必填 必须填写有效的电子邮件地址
字段为必填 值无效或太长
字段为必填 必须填写有效的电子邮件地址