Перейти к содержанию

Simulate the behavior of layered composite analysis structures and their progressive degradation.

Composites

In the quest to make products lighter yet stronger, manufacturers are increasing their use of composite materials. It is also prohibitively expensive to create prototypes of products made from composites, so simulation must play a key role in the development of new products using laminate composite materials. Simcenter is at the leading-edge of composites analysis through continuous development of material models and element types. Simcenter speeds the entire process for simulating laminate composite materials through a seamless connection to composites design, accurate solvers and comprehensive post-processing.

Composites

In the quest to make products lighter yet stronger, manufacturers are increasing their use of composite materials. It is also prohibitively expensive to create prototypes of products made from composites, so simulation must play a key role in the development of new products using laminate composite materials. Simcenter is at the leading-edge of composites analysis through continuous development of material models and element types. Simcenter speeds the entire process for simulating laminate composite materials through a seamless connection to composites design, accurate solvers and comprehensive post-processing.

Вас интересует [[global-preference-center-interest-placeholder]]?

Подпишитесь на обновления [[global-preference-center-interest-placeholder]]

Что-то пошло не так.

К сожалению, не удалось сохранить отправленную информацию. Повторите попытку.

Благодарим Вас за регистрацию. Подписываетесь первый раз? Пожалуйста, проверьте свою электронную почту и подтвердите подписку.

Это обязательное поле Укажите действующий электронный адрес
Это обязательное поле Недопустимое значение, либо превышено допустимое число символов
Это обязательное поле Укажите действующий электронный адрес