1. Home
Press Release

Latest release brings engine combustion modeling to Simcenter STAR-CCM

October 30, 2019
Plano, TX

Simcenter STAR-CCM+ simulation of combustion in a gasoline direct injection engine.

Siemens Digital Industries Software announces the latest release of Simcenter™ STAR-CCM+™ software, which includes new physics models that allow engineers to increase the realism and fidelity of their simulations. The new release includes the hotly anticipated combustion capability and time-saving tools that allow engineers to make better decisions in hours instead of weeks.

  • The new combustion modeling capability allows engineers to quickly and easily assess the performance of gasoline direct-injection engines and automatically run engine speed and load sweeps for the generation of digital performance maps.
  • All practical flow problems involve the interaction between fluids and solids. The new direct coupling between Simcenter STAR-CCM+ and Simcenter™ NASTRAN® software enables users of either tool to directly account for the effects of fluid-structure-interaction, reducing the need for overly conservative design choices. 
  • Refraction and radiation are especially important when considering the design of modern headlamps, which have multiple radiation emitting sources. These, along with the sun, can create hot spots as the light is reflected and refracted. The newly implemented Photon-Monte-Carlo is a statistical method for solving this type of radiation problem and is significantly faster and more accurate than alternative approaches.

For more information on Simcenter STAR-CCM+, please click here

Siemens Digital Industries Software is driving transformation to enable a digital enterprise where engineering, manufacturing and electronics design meet tomorrow. Our solutions help companies of all sizes create and leverage digital twins that provide organizations with new insights, opportunities and levels of automation to drive innovation. For more information on Siemens Digital Industries Software products and services, visit sw.siemens.com or follow us on LinkedIn, Twitter, Facebook and Instagram. Siemens Digital Industries Software – Where today meets tomorrow.

Note: A list of relevant Siemens trademarks can be found here. Other trademarks belong to their respective owners.

Contacts for Press

Siemens Digital Industries Software PR Team
press.software.sisw@siemens.com