04 June 2018

Mentor extends Capital for efficient design of SAE J1939-based CAN networks

New Capital® Systems Networks™ product boosts design efficiency for J1939-based CAN networks by up to 90 percent by enabling a generative design approach.

Mentor, a Siemens business, today introduced Capital® Systems Networks™ – an advanced software tool engineered to speed and simplify the creation of in-vehicle Controller Area Network (CAN) communications networks based on the SAE J1939 standard. The solution provides proven, powerful technology to help engineers rapidly develop, optimize and validate J1939 networks.

Commonly deployed in heavy-duty commercial vehicles such as trucks, buses and off-road vehicles, SAE J1939 is a data networking standard used for in-vehicle communications and diagnostics. Commercial vehicles may incorporate as many as six separate CAN networks, requiring new designs and rework for each new vehicle model.

As the number of processors, sensors, and electronic actuators deployed in commercial vehicles rises with each model-year, so too does the complexity of designing the data networks used to connect them. Despite this rising complexity, a lack of robust network design tools often forces engineers to rely on rudimentary, maintenance-intensive technologies such as spreadsheets incorporating in-house macros.

Designed to address these challenges, the Capital Systems Networks product enables holistic network development. As part of the extensive Capital tool suite, the new Mentor tool integrates network and electrical design within a single environment, streamlining development of functional and physical designs for J1939 networks. By supporting a generative design process within a coherent electric and electronic (E/E) architecture, Capital Systems Networks helps dramatically speed network design, validation and optimization.

The Capital Systems Networks tool includes a robust library and unified dictionary of SAE J1939 signals, functions and features. This allows designs, ECUs, and even entire networks to be reused and tailored for specific vehicle models and variants.

“Capital Systems Networks is a sophisticated tool that addresses the massive complexity associated with today’s automotive network designs,” said Martin O’Brien, vice president and general manager of Mentor’s Integrated Electrical Systems Division. “Designed for optimal scalability and re-usability, Capital Systems Networks’ model-based solution enables a generative design approach offering the potential for 90 percent design efficiency improvement for J1939-based CAN networks, while at the same time handling several thousands of signals.”

“Capital supports advanced platform architecture exploration, allowing us to generate rapid iterations and evaluate different implementation options directly within the design environment,” said Rosa Talarico, CVPD ES system integration, networking & methodologies manager for CNHi. “This functionality, together with Capital’s data reusability and scalability across multiple abstractions, allows us to dramatically reduce design cycles and speed time to market.”

About Capital
Developed for transportation applications, Mentor’s Capital Electrical Design Software suite spans an extended flow from concept and electrical architecture definition to wire harness design, manufacture and vehicle maintenance. Combining powerful design automation and modern enterprise integration capabilities, the software creates digital continuity within the electrical domain to compress development cycle time and deliver significant cost reductions. Capital tools can be implemented individually or deployed together in a unified flow that seamlessly matures data within a consistent environment. Robust integration with adjacent domains (such as MCAD and PLM) is fully supported, as is cross-organizational collaboration.

Availability
Capital Systems Networks is available now. For more information please visit http://go.mentor.com/4ZK6f.

Основное контактное лицо

James Price
503.685.1778
james_price@mentor.com