28 May 2019

Siemens launches Capital Load Analyzer software to reduce aerospace electrical compliance and certification risk

Siemens announces today that its Mentor business has introduced the CapitalTM Load Analyzer software product to help simplify aircraft electrical design compliance and certification. Modern aircraft systems, such as electrical flight control systems and in-flight entertainment systems, require more power, have more electrical content, and have higher compliance risk due to increased complexity. According to market research firm Bishop & Associates Inc., for 2019 the market for commercial air cable/harness assemblies is projected at approximately $2.4 billion, growing to $3.3 billion in 2024, with CAGR just over 6.5%.  The new Capital Load Analyzer is the industry’s first electrical systems technology that leverages automation and digital data continuity to facilitate regulatory compliance.

Current methods for verification and analysis rely on fragmented data, and are typically conducted manually using drawings and spreadsheets, after the major electrical design work is complete. Uncovering problems during this late program phase forces costly design iterations and missed critical milestones, such as Customer Acceptance and Type Certification, impacting aircraft revenue recognition.

To mitigate such risks, the new Capital Load Analyzer product draws upon the electrical digital twin, generated from the overall power system and subsystems design, to predict the aircraft’s electrical power demand. The digital twin, native to the Capital product, is an accurate, up-to-date version of the electrical system as it evolves during the development process. The electrical digital twin provides an automated view of the entire power system, enabling engineers to design for compliance from the very beginning of the project. Analysis and simulation are performed using primary design data instead of using traditional disconnected approaches. Rules-based checking and analysis helps enable accurate and complete verification for aircraft power system efficiency for each flight phase – even under load shedding for emergency conditions.

“By leveraging the new Capital Load Analyzer, we anticipate engineers will be able to mitigate risk in a variety of certification types to meet airline safety requirements,” according to Dick Slansky, ARC Advisory group senior analyst.  “Electrical systems for new aircraft have become much more complex to meet the ever increasing demands of advanced avionics and expanded cabin amenities.  Creating an electrical digital twin using Capital Load Analyzer at all phases of the aircraft’s product lifecycle could result in considerable time and costs savings while achieving higher-performance electrification of today’s aircraft.”

Data Management for Comprehensive Analysis and Reporting

Capital Load Analyzer automatically extracts all electrical load analysis data into the user’s own reporting template for easy and efficient report generation. This technology pulls data directly from the digital twin so the user can see the impact of design changes at any time and at any stage of the design process. The ability to quickly generate real-time reports enables users to monitor design tasks and identify potential issues early in the design process, thereby mitigating program risk. The Capital Load Analyzer product reports compliance analysis results for each design configuration and variant.  

“Capital Load Analyzer is a true electrical collaboration platform that provides the digital continuity required across a broad range of critical tasks for electrical systems compliance and certification,” stated Martin O’Brien, senior vice president, Integrated Electrical Systems, Siemens Digital Industries Software. “Capital’s digital thread allows aerospace electrical system designers to deploy an automated design-for-compliance methodology with greater efficiency, improved product quality and a competitive advantage“

Siemens is further extending the Capital product line to include two additional technologies. A new wire derating product optimizes the aircraft’s wire sizes to reduce weight while maintaining integrity against hazards, such as over-heating. And the new 3D signal separation tool evaluates the electrical design against safety-critical design considerations, such as power routing requirements and harness spacing for redundant systems. These products ship in the second half of 2019.

All of these new technologies will also be showcased at the Siemens Detroit Realize Live user conference (June 10 – 13, 2019) and the International Paris Air Show, Le Bourget (June 17-23, 2019) in the Siemens Chalet. For more information, visit the product website: www.mentor.com/aerospace 

Siemens Digital Industries Software, a business unit of the Siemens Digital Factory Division, is a leading global provider of software solutions to drive the digital transformation of industry, creating new opportunities for manufacturers to realize innovation. With headquarters in Plano, Texas, and over 140,000 customers worldwide, Siemens Digital Industries Software works with companies of all sizes to transform the way ideas come to life, the way products are realized, and the way products and assets in operation are used and understood. For more information on Siemens PLM Software products and services, visit www.siemens.com/plm.

Основное контактное лицо

Suzanne Graham
503.685.7789
suzanne_graham@mentor.com