26 October 2016

Mentor Graphics Introduces FloEFD Frontloading Fully-Embedded Computational Fluid Dynamics (CFD) Solution for Solid Edge

WILSONVILLE, Ore., October 26, 2016 – Mentor Graphics Corporation (NASDAQ: MENT) today announced the only fully-embedded computational fluid dynamics (CFD) solution for Solid Edge® software, a mainstream computer-aided design (CAD) solution developed by Siemens’ product lifecycle management (PLM) software business. Solid Edge customers can now take advantage of Mentor Graphics® FloEFD™ frontloading CFD product to simulate fluid flow in their design process. The FloEFD solution is especially well suited for use during the design process as it reduces overall time to a solution by as much a 65%-75% compared to other CFD tools.

Mentor Graphics’ award-winning FloEFD CFD solution automates the most onerous CFD steps which include transferring model geometry to the CFD application, modeling internal cavities if needed and creating a “mesh.” The FloEFD CFD technology takes the geometry directly from the CAD application, automatically performs the necessary translations and cavity modeling, and generates an optimized mesh before executing analysis. This approach provides accurate analysis results quickly thus enabling designers to validate their designs early and often. It also allows the designer to explore a succession of ideas without risking project deadlines.

“FloEFD for Solid Edge is a leap forward for our customers who need to do flow analysis on their engineering projects,” said Dan Staples, vice president, Solid Edge product development, Siemens PLM Software. “This tool allows engineers to quickly run various 'what if’ scenarios and optimize their design directly inside of the Solid Edge window.”  

Key Features of the FloEFD for Solid Edge Product:

The new FloEFD product for Solid Edge helps companies conduct analysis earlier in the design process. Engineers can operate within their preferred and familiar mechanical CAD (MCAD) interface thus reducing design cycle times by order of magnitude compared to traditional methods and tools, while increasing design quality:

  • Robust 3D fluid flow and heat transfer analysis software capable of solving complex real-life engineering problems.
  • Fully-embedded in Solid Edge, FloEFD technology allows users to conduct multiple design studies and evaluate how the modifications influence the design performance immediately.
  • Features an intuitive user interface with built-in intelligent automation including real-time feedback and timely outputs that can be generated quickly in Microsoft Word and Excel.
  • Parametric study enables user to compare a wide range of project variations.
  • Fast, automated SmartCell™ meshing technology to create realistic simulations for complex 3D models including rotating equipment and transient flow behaviors – providing unprecedented speed-up in the overall design process.

"Mentor’s FloEFD frontloading CFD technology full-featured 3D analysis eliminates workflow complexity and meshing overheads compared to other available CFD software,” said Roland Feldhinkel, general manager of Mentor Graphics Mechanical Analysis Division. “We believe Solid Edge customers will reap tremendous value in using our FloEFD solution for CAD-centric CFD design and performance optimization, while reducing time and costs to meet their product delivery goals.” 

FloEFD for Solid Edge is now available for shipment. For additional information about FloEFD for Solid Edge, please go to: https://www.mentor.com/products/mechanical/floefd/floefd-solid-edge/

Mentor Graphics and Mentor are registered trademarks, and FloEFD is a trademark of Mentor Graphics Corporation. All other company or product names are the registered trademarks or trademarks of their respective owners.

Solid Edge is a trademark or registered trademark of Siemens Product Lifecycle Management Software Inc. or its subsidiaries in the United States and in other countries.

Основное контактное лицо

Larry Toda
503.685.1664
larry_toda@mentor.com