Software Engineering

Our Software Engineering solution for the Heavy Equipment Industry leverages an Integrated product development strategy, where software (both embedded and non-embedded) development is part of a multi-discipline approach, enabling closed-loop performance assessment. Providing bi-directional integration between ALM and PLM which helps to build the complete digital twin.

Our Software Engineering solution for the Heavy Equipment Industry leverages an Integrated product development strategy, where software (both embedded and non-embedded) development is part of a multi-discipline approach, enabling closed-loop performance assessment. Providing bi-directional integration between ALM and PLM which helps to build the complete digital twin.

Learn More

Software related quality problems are emerging as a major source of recalls and warranty claims. This is partly due to the difficulty of understanding the requirements, a solid integrated development environment and testing the software applications in all conditions and updating software in the field. The costs of claims will rise significantly without a software management process that manages quality across software programming domains. 

Within the last decade or so, there has been an exponential increase in the products with embedded software in the Heavy Equipment Industry. Management of software changes caused by these mechanical, electrical and electronics changes is complex and companies need to drive the changes and impact analysis in a concurrent fashion across-domains delivering product quality, compatibility and engineering accountability. 

It is estimated that embedded systems contribute to more than 90% innovations and new features driving the overall product quality and increased dependency on software delivery. As software engineering continues to evolve, it has become apparent that no single tool can fulfill all the needed process tasks to effectively deliver the full software application and a robust ALM tool is needed to help orchestrate all the needed process tasks with relevant extensions needed. Our 

Software Engineering solution allows you to transform otherwise disconnected tools and processes into an integrated design solution that enables you to builds the complete digital twin by combining software functionality with mechanical and electrical capabilities and aligns the product through development and change impact analysis.

Запись вебинара

Гибкое ALM для менеджеров проектов: канбан, приборные панели, отчеты и отслеживаемость

Совместная работа в реальном времени, единое хранилище данных, отслеживаемость по разным инструментам и проектам, более удобное наблюдение за проектами и составление отчетов — все это помогает разрабатывать и выпускать более качественное программное обеспечение в более сжатые сроки.

Посмотреть вебинар

Возможности решения

Explore the key areas of this solution.

Aero - DO-178C

Uncouple complex development processes at the work item level to accelerate innovative development while at the same time easing proof of compliance with DO-178C.

Auto - Functional Safety - ISO26262

Accelerate Functional Safety compliance for ISO 26262, Automotive SPICE and CMMI standard.

Bill of Materials Management

Manage software assemblies in context of the equipment and build sophisticated machinery variants based on customer and global manufacturing requirements.

Extensions

Comprehensive tools-eco-system that suits ALM needs across code-management, performance, test automation and build-automation.

ISO14971

Comprehensive, automated history of all artifacts facilitates proof of compliance - Integrate risk management processes leveraging the ISO 14971 template.

PLM-ALM Integration

Drive the changes and impact analysis in a concurrent fashion across-domains delivering product quality, compatibility, traceability and engineering accountability.

Product Requirements Engineering

Capture and manage product requirements with their decomposition and cascade to high level software requirements and specifications.

Software Agile/Hybrid Project Management

Out-of-the-box project templates are available and can be adjusted to either modern agile techniques or traditional methods.

Software Audits, Metrics & Reports

Improve decision-making and project execution with detailed analytics and real-time status reports.

Вас интересует [[global-preference-center-interest-placeholder]]?

Подпишитесь на обновления [[global-preference-center-interest-placeholder]]

Что-то пошло не так.

К сожалению, не удалось сохранить отправленную информацию. Повторите попытку.

Благодарим Вас за регистрацию. Подписываетесь первый раз? Пожалуйста, проверьте свою электронную почту и подтвердите подписку.

Это обязательное поле Укажите действующий электронный адрес
Это обязательное поле Недопустимое значение, либо превышено допустимое число символов