Inovação e gerenciamento de programa sincronizado e colaborativo para novos programas
Aeroespacial e Defesa
Inovação e gerenciamento de programa sincronizado e colaborativo para novos programas
Explorar o SetorAutomotivo e Transporte
Integration of mechanical, software and electronic systems technologies for vehicle systems
Explorar o SetorProdutos de Consumo e Varejo
A inovação de produtos através do gerenciamento eficaz de formulações, embalagens e processos de manufatura integrados
Explore o SetorEletrônicos e Semicondutores
O desenvolvimento de novos produtos aproveita dados para melhorar a qualidade e a lucratividade e reduz custos e tempo de introdução no mercado
Explore o SetorEnergia e Utilidades
Supply chain collaboration in design, construction, maintenance and retirement of mission-critical assets
Explorar o SetorHeavy Equipment
Construction, mining, and agricultural heavy equipment manufacturers striving for superior performance
Explore IndustryMáquinas Industriais e Equipamento Pesado
Integration of manufacturing process planning with design and engineering for today’s machine complexity
Explorar o SetorInsurance & Financial
Visibility, compliance and accountability for insurance and financial industries
Explore IndustryMarinha
Inovação na construção naval para reduzir de maneira sustentável o custo do desenvolvimento de frotas futuras
Explore o SetorMedia & Telecommunications
Siemens PLM Software, a leader in media and telecommunications software, delivers digital solutions for cutting-edge technology supporting complex products in a rapidly changing market.
Explore IndustryDispositivos Médicos e Farmacêuticos
“Inovação de produtos personalizados" através da digitalização para atender a demandas do mercado e reduzir custos
Explore o SetorSmall & Medium Business
Remove barriers and grow while maintaining your bottom line. We’re democratizing the most robust digital twins for your small and medium businesses.
Explore IndustryImproving power electronics thermal design and reliability using test and simulation
Improving power electronics thermal design and reliability using test and simulation
How to apply thermal transient testing, electronics cooling simulation and accurate model calibration to improve thermal design
For compact design of reliable power electronics modules in applications such as vehicle electrification, rail, aerospace and power conversion - thermal management at component to module level must be evaluated carefully during development. This presentation introduces a method for combining use of multiple thermal measurements of IGBT power semiconductors within a power module, with calibration of detailed compact thermal models for use in improving the accuracy of module level electronics cooling simulation studies.
This approach presented uses Simcenter T3STER thermal transient test technology for heat flow path analysis of a power semiconductor package in conjunction with automatic detailed package model calibration and subsequent system level thermal simulation possible with Simcenter Flotherm or Simcenter FLOEFD software.
The presentation also briefly reviews thermal reliability test strategies using combined power cycling and failure diagnosis via thermal transient test methods (using Simcenter POWERTESTER).
Presenter: Andras Vass-Varnai
Você aprenderá:
Olá Bob (será substituído com o primeiro nome real durante a visita do site real)
Queremos saber mais sobre você.
Olá Bob (será substituído com o primeiro nome real durante a visita do site real)
Você tem acesso a este webinar por 90 dias. Clique abaixo para iniciar a visualização.
How to apply thermal transient testing, electronics cooling simulation and accurate model calibration to improve thermal design
For compact design of reliable power electronics modules in applications such as vehicle electrification, rail, aerospace and power conversion - thermal management at component to module level must be evaluated carefully during development. This presentation introduces a method for combining use of multiple thermal measurements of IGBT power semiconductors within a power module, with calibration of detailed compact thermal models for use in improving the accuracy of module level electronics cooling simulation studies.
This approach presented uses Simcenter T3STER thermal transient test technology for heat flow path analysis of a power semiconductor package in conjunction with automatic detailed package model calibration and subsequent system level thermal simulation possible with Simcenter Flotherm or Simcenter FLOEFD software.
The presentation also briefly reviews thermal reliability test strategies using combined power cycling and failure diagnosis via thermal transient test methods (using Simcenter POWERTESTER).
Presenter: Andras Vass-Varnai
Você aprenderá: