Ir para o Conteúdo

Plano, Texas and Berlin, Germany, 23 October 2017

Siemens’ latest release of Simcenter 3D advances computer-aided engineering and simulation

  • Powerful generative design workflows support fully integrated topology optimization and Convergent Modeling for efficient design and simulation
  • Advanced solutions deliver on Simcenter strategy for structural dynamics, motion and acoustics, delivering superior functionality and performance
  • Improved industry workflows include universal connections support for efficient modeling of large assemblies

Siemens announces the latest version of Simcenter 3D, its flagship environment for multi-disciplinary computer-aided engineering (CAE), with new comprehensive solutions across multiple simulation disciplines. Simcenter 3D is an advanced stand-alone CAE application for analysts and discipline experts that works with data from any CAD source. Because it is built on the Siemens NXTM platform, it also works seamlessly with NX CAD. With more enhancements than any previous release, Simcenter 3D, part of Siemens’s SimcenterTM portfolio of simulation and test solutions for predictive engineering analytics, looks to revolutionize how simulation engineers can help drive design direction in industries such as automotive, aerospace and industrial machinery.

This latest release provides topology optimization solutions that work seamlessly with Convergent Modeling™ technology to provide comprehensive generative design workflows. These solutions allow for more accurate motion modeling, and more efficient acoustic and structural dynamics simulations. Simcenter 3D now provides expanded support for general purpose nonlinear solutions based on the NX Nastran multi-step nonlinear solver as well as advanced analysis of composites based on LMS Samtech Samcef™ software. This latest release also delivers several enhancements to improve industry workflows across a wide range of industries, for modeling connections in large assemblies as well as accurate simulation of flexible pipes and hoses.

“Siemens is executing on the Simcenter strategy it announced last year as evidenced by its ongoing investment in new simulation capabilities along with the accelerated integration of CAE technologies acquired over the past several years. The latest release of Simcenter 3D delivers innovative capabilities for topology optimization applied in the context of generative design and also brings together unique hybrid test/analysis technologies that extend the ability to model and simulate system dynamics for complex applications such as high frequency noise and vibration,” said Donald Tolle, practice director, Simulation-Driven Systems Development at CIMdata. “These product enhancements ensure that Simcenter 3D will continue to be a robust, scalable, and multi-disciplinary CAE environment for simulation and analysis specialists.”

Working seamlessly with NX CAD and Convergent Modeling technology, Simcenter 3D now offers generative design solutions for designers and advanced analysts. For the first time, output from a topology optimization process can be utilized directly in the design process, without the need to recreate geometry. Furthermore, engineers can now work directly with scanned data or an optimized shape to conduct more detailed simulations to ensure performance. By using Simcenter 3D along with HEEDS™ software for design exploration automation, engineers are able to fully explore the design space and generate innovative designs that meet more stringent design requirements.

New with this release, hybrid modeling allows analysts to incorporate test-based data into their simulation models to achieve better accuracy within the simulation. Other enhancements include support for modeling sub-mechanisms within motion assemblies, faster computation time for analytical contact in motion models, and improved performance for interior and exterior acoustics simulation.

Nonlinear simulation in Simcenter 3D is greatly expanded by leveraging enhancements in NX Nastran and integrating capabilities from the LMS Samcef solver. In addition to the already strong capabilities for simulating nonlinear thermo-mechanical behavior in turbomachinery, Simcenter 3D now offers expanded support for general purpose nonlinear simulation with more elements, greater robustness and algorithms for multi-step nonlinear simulation to provide enhanced realism and faster solution times. Additionally, support for curing simulation of composites now allows prediction of residual stresses and spring-back effects.

Several of the enhancements target industry-specific workflows. Simulation engineers in automotive, aerospace, and heavy machinery companies benefit from the integration of universal connections support, which can help to efficiently build large system models with many connections and solve across several solvers. Simcenter 3D also leverages the LMS Samcef solver for simulation of flexible pipes and hoses which are commonly used in a variety of industries.

“Our Simcenter solutions deliver critical capabilities that help our customers engineer innovation into their products,” said Jan Leuridan, senior vice president for Simulation and Test Solutions, Siemens PLM Software. “With our latest release of Simcenter 3D we are able to integrate multiple technologies from different tools all under one platform. Capitalizing on our deep experience in geometry-based CAE as well as our strength in key disciplines such as structural dynamics, acoustics, motion, and nonlinear analysis, we have enhanced Simcenter 3D to enable more streamlined workflows and a broader set of simulations in support of performance engineering.”

For further information on Simcenter 3D, please see www.plm.automation.siemens.com/en/products/simcenter/3d/v12/index.shtml.

Siemens PLM Software, a business unit of the Siemens Digital Factory Division, is a leading global provider of software solutions to drive the digital transformation of industry, creating new opportunities for manufacturers to realize innovation. With headquarters in Plano, Texas, and over 140,000 customers worldwide, Siemens PLM Software works with companies of all sizes to transform the way ideas come to life, the way products are realized, and the way products and assets in operation are used and understood. For more information on Siemens PLM Software products and services, visit www.siemens.com/plm.

Follow us on Twitter at:www.twitter.com/siemens_press

Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world’s largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com/plm.

Note: Siemens and the Siemens logo are trademarks or registered trademarks of Siemens AG. Simcenter, NX and Convergent Modeling are trademarks or registered trademarks of Siemens Product Lifecycle Management Software Inc. or its subsidiaries in the United States and in other countries. NASTRAN is a registered trademark of the National Aeronautics and Space Administration. HEEDS is a trademark or registered trademark of Red Cedar Technology, Inc. LMS is a trademark or registered trademark of Siemens Industry Software NV or any of its affiliates. LMS Samtech Samcef is a trademark or registered trademark of Siemens Industry Software NV or any of its affiliates. All other trademarks, registered trademarks or service marks belong to their respective holders.

Contato Principal

Natalie Navales
+1 314 264 8671
natalie.navales@siemens.com