Ir para o Conteúdo

Plano, TX, 19 October 2016

Siemens to revolutionize product development with end-to-end additive manufacturing solution

  • World’s first offering to integrate entire additive manufacturing process from automated performance-driven design optimization to advanced 3D printing
  • Generative design, enabled by Convergent Modeling and topology optimization, yields organic shaped parts optimized for performance and 3D printing
  • Smart product models to be used from design through simulation and production with no need for data conversion
  • Ability to “reshape everything” could significantly reduce costs, increase product performance, dramatically impacting products in many industries

Siemens’ product lifecycle management (PLM) business announces a new comprehensive solution to unleash the full potential of the burgeoning additive manufacturing revolution. The new solution, which will begin rolling out in January, 2017, is comprised of integrated design, simulation, digital manufacturing, data and process management software. The new set of offerings will help companies fully leverage the benefits of the latest additive manufacturing technology, also known as 3D printing. The integrated solution will use smart product models through all phases without the need for conversion or translation between applications or processes. The solution will enable automated generative design using the new topology optimization capabilities which often result in organic shapes that would be difficult for a human designer to envision, and impractical or impossible to produce with traditional manufacturing techniques. This technology, combined with Siemens’ new advanced additive manufacturing software, could enable companies to reshape everything for optimal performance at a reduced cost. In addition, the ability to 3D print an optimized part shape could reduce the number of parts in an assembly, thereby decreasing weight and increasing strength. As a result, industries such as automotive, aerospace and medical devices could realize dramatic value.

“Siemens PLM Software is pushing the additive manufacturing envelope by developing solutions to help create functionally optimized geometry that is inconceivable based on conventional design and manufacturing methods,” said Dr. Ken Versprille, Executive Consultant, CIMdata. “Previously unsolvable design and manufacturing challenges are now quite feasible with these new software and production technologies. Siemens PLM Software has a vision for how the technology fits together from end-to-end and is putting that vision in place to move the industry forward.”

Designers are trained to create parts with traditional production technologies in mind, which can limit creativity and innovation. Today, production parts are either stamped, molded, cast or machined. By providing engineers and designers with a completely new way to design and manufacture parts, Siemens is helping them reimagine the next generation of products. Companies can create unique, better performing designs with significantly increased strength/weight ratios and apply advanced integrated simulation and analysis technology to predict design performance. This new transformative technology will help increase design innovation.

“In order to make additive manufacturing a true industrial production process, manufacturers need to have seamless digital integration across design, production and automation, including control and monitoring of machine performance,” said Joachim Hoedtke, CEO, Hoedtke GmbH & Co. KG, an innovator in additive manufacturing and Siemens customer. “Siemens is bringing together multiple software tools with new technologies focused on additive manufacturing to help companies accomplish this goal.”

The new additive manufacturing solution will include Siemens’ NX™ software, an integrated computer-aided design, manufacturing and engineering (CAD/CAM/CAE) solution, the newly announced Simcenter™ portfolio, a robust suite of simulation software and test solutions, Teamcenter® software, the world's most widely used digital lifecycle management system, and SIMATIC IT Unified Architecture Discrete Manufacturing and SIMATIC WinCC, two elements of Siemens’ recognized Manufacturing Operations Management (MOM) portfolio for production execution and manufacturing automation.

Two of the new technologies included in the solution that enable automated generative design, are Convergent Modeling and topology optimization. Convergent Modeling, which was announced with the latest release of NX, is the first technology of its kind. It will help engineers optimize part design for 3D printing, speed up the overall design process and provide scan-to-print functionality, which makes reverse engineering more efficient. It is a brand new modeling paradigm that greatly simplifies the ability to work with geometry consisting of a combination of facets, surfaces and solids, without the need for time-consuming data conversion. Topology optimization, another new technology will help analysts automate the iterative process for designing and optimizing parts for multi-physics performance including vibration, fluid dynamics and heat transfer. The integrated simulation and predictive engineering analytics capabilities help evaluate the design for manufacturability to provide greater confidence needed to move forward with designs optimized for additive manufacturing.

In addition to these new technologies, Siemens is also introducing a new 3D print preparation solution for both metal and plastic parts that will use the same smart product models from the design and simulation phase to help automate design changes and streamline the entire process. The new solution assists operators in preparing parts for powder bed and multi jet fusion printing. For 3D printed metal parts, NX provides model preparation for laser metal deposition and NC programming. This includes simulation for hybrid additive machine tools, where metal deposition is incorporated with subtractive methods in a single machine tool environment. For extruded materials such as plastics and carbon fiber reinforced nylon, a new multi-axis robotic fused deposition modeling (FDM) programming technology has been developed and is being field tested. After parts are printed, the same integrated NX system is used for post-printing NC operations such as intuitively programming the removal of support structures, machining of precision surfaces and other processing and inspection operations.

“This is just the beginning of a new generation of manufacturing capabilities, and Siemens is focused on delivering software technology to support an optimized end-to-end process with tools such as Convergent Modeling, topology optimization and 3D print preparation that are developed specifically to industrialize additive manufacturing,” said Tony Hemmelgarn, president and CEO, Siemens PLM Software. “Siemens continues to invest in innovation and work with technology partners to develop new solutions to drive advances in additive manufacturing capabilities to make the 3D printing of production parts a reality.”

For further information on Siemens PLM Additive Manufacturing, please visit: www.siemens.com/plm/additivemanufacturing

Follow us on Twitter at www.twitter.com/SiemensPLM.

Contato Principal

Salim Rahimi
+1 972 987 3206
salim.rahimi@siemens.com