Innovation and collaborative, synchronized program management for new programs
Advanced Planning software is a strategic decision tool designed to aid you in long and mid-term planning. It considers forecast and long-term orders, supports decision making about the feasibility and affects the general direction of productions.
Advanced planning software supports major production capacity decisions surrounding extending the work force, resource capacity, and factories. It helps you determine what and how much to make, where and when to make it, and exactly what materials and resources are required.
Planning can be executed in finite or infinite capacity mode and planning time periods can be days, weeks, months, or a combination of all three. If used together with our advanced scheduling system, detailed production schedule information can be sent back to the planning system to override planned volume with scheduled volume. Master Production Schedule (MPS) can then be re-calculated using production schedule as the base for new results.
Advanced Planning software is a strategic decision tool designed to aid you in long and mid-term planning. It considers forecast and long-term orders, supports decision making about the feasibility and affects the general direction of productions.
Advanced planning software supports major production capacity decisions surrounding extending the work force, resource capacity, and factories. It helps you determine what and how much to make, where and when to make it, and exactly what materials and resources are required.
Planning can be executed in finite or infinite capacity mode and planning time periods can be days, weeks, months, or a combination of all three. If used together with our advanced scheduling system, detailed production schedule information can be sent back to the planning system to override planned volume with scheduled volume. Master Production Schedule (MPS) can then be re-calculated using production schedule as the base for new results.
The planning Bill of Materials (BOM) can be exploded, and then the production plan for lower level items is calculated in the same way. Based on the MOM explosion and the production plan, proposed material purchase requirements can be exported to an ERP system or Excel for action.
Once an initial Master Production Schedule (MPS) has been created, data can be displayed as stock profile graphs and capacity usage graphs. The MPS can be changed by simply clicking and dragging a point on the stock or capacity graphs, and the production of a particular item can be moved from one planning period to another. Any changes made will be reflected in all the linked plot and grid windows.
In a make-to-order environment, stock levels of finished and intermediate items will not be part of the key process parameters. But there will still be the need to evaluate the effects of future demand changes on the manufacturing process. When a change in demand occurs, whether in terms of quantity or delivery dates, there is a need to be able to quickly assess if it is possible to meet the new requirements.
In a make-to-stock environment, you can generate accurate and achievable master production schedules (MPS) considering rough cut capacity, pack forward figures, target days of stock cover, manufacturing preferences, minimum and maximum re-order quantities, re-order multiples and product shelf life. Production capacity can be specified as a quantity, duration or weight. By using the Preactor calendar system capacity, production capacity can be varied over time. The capacity available then limits the production volume created in each period.