Innovation and collaborative, synchronized program management for new programs
Teamcenter Requirements verification and validation capabilities help close the loop on requirements by capturing and associating verification and validation results with requirements while enabling focused testing. With Teamcenter Requirements Management, requirements are included in a closed loop process, where requirements are tied to how they are verified and validated (V&V). Because Teamcenter also includes test and validation management, requirements can be tied to test cases that validate them.
As a result, you get full visibility into requirements verification and validation processes, along with the status of current V&V efforts, and any issues generated during testing. Test results in-turn feed standard workflow, change and other processes to manage compliance issues (as well as maintain evidence of compliance for auditing purposes). This sets up an organization for significant V&V productivity improvements.
Teamcenter Requirements verification and validation capabilities help close the loop on requirements by capturing and associating verification and validation results with requirements while enabling focused testing. With Teamcenter Requirements Management, requirements are included in a closed loop process, where requirements are tied to how they are verified and validated (V&V). Because Teamcenter also includes test and validation management, requirements can be tied to test cases that validate them.
As a result, you get full visibility into requirements verification and validation processes, along with the status of current V&V efforts, and any issues generated during testing. Test results in-turn feed standard workflow, change and other processes to manage compliance issues (as well as maintain evidence of compliance for auditing purposes). This sets up an organization for significant V&V productivity improvements.
As requirements are defined, they begin to drive program execution plans needed to fulfill them (resources, schedules, tasks, deliverables, etc.) Requirements managed in Teamcenter are tied directly to program milestones and project tasks, allowing for progress and exceptions monitoring. Once requirements are established, and the programs they are tied to begin to execute, you have complete visibility into the processes around requirements, test cases, resources, etc., allowing you to address program risk proactively.
Teamcenter manages test cases and test procedures, and requirements can be linked directly to tests that validate them. Test cases are tied to requirements as they are defined to assess requirement completeness, enabling test case reuse that sets up “change-focused testing”, rather than testing everything. Traceability between requirements and test cases solves this problem by only testing the requirements that have changed—saving time and money. You have complete coverage backed by actual test results.
Siemens Healthcare uses Teamcenter to increase design re-use
See all Success StoriesWebinar na żądanie | 13 min.
Przekonaj się o kluczowym znaczeniu powiązanych wymagań, które pozwalają wdrażać innowacje i poznaj nasze zintegrowane podejście do kompleksowego rozwoju produktu.
Przekonaj się o kluczowym znaczeniu powiązanych wymagań, które pozwalają wdrażać innowacje i poznaj nasze zintegrowane podejście do kompleksowego r...
Watch this video to learn how to balance the needs of engineering, and the business in general, when choosing product lifecycle management software.
Reach more people and processes for greater business performance.
See how easy it is to capture, share, and maintain requirements. And more importantly, to connect them to your product development processes to ens...