Marine Craft Design

Enter the summary here - no longer than 75 - 150 words. Use two paragraphs if the text is over 75 words. This is the full version of the summary text which will appear on the full version of the solution page.
Enter the summary here - no longer than 75 - 150 words. Use two paragraphs if the text is over 75 words. This is the full version of the summary text which will appear on the full version of the solution page.

Learn More

Enter the details here - Long version of what this solution does. This is displayed on the solution page in the Learn More block.

Webinar na żądanie

Symulacja dla konstruktorów na platformie Creo

Symulacja dla konstruktorów na platformie Creo

Zobacz, jak użytkownicy Creo mogą prowadzić symulacje

Obejrzyj webinar

Możliwości rozwiązania

Explore the key areas of this solution.

Adaptable Integrated BOM

Leverage a flexible BOM management strategy that enables a single, accurate product definition for all who interact with the BOM. With flexibility in how you define and manage your BOM, you can provide a complete, up-to-date source of information that eliminates the need for standalone spreadsheets and systems. Teamcenter® supports up-front planning and master product definition, through design, development, manufacturing, service and more.

Aero Structures Design

With integrated tools to go from Concept to Detailed Design to Analysis to Manufacturing and beyond, NX can help the customer better meet or exceed the demand pressure from the airlines by accelerating design productivity. NX enables more design iterations in less time, resulting in bringing a better product to market faster.

Automotive Design

Changing consumer preferences and regulatory pressures are forcing automotive companies to find new ways to improve vehicle performance and design. These pressures profoundly impact the design and engineering processes. NX provides a full suite of design tools that work within a fully integrated product development system from concept design through manufacturing.

CAE Simulation

Adopt a compromise-free approach to physics modeling using best-in-class simulation tool

Composite Design and Manufacturing

Automatically generate composite manufacturing data — such as flat patterns and data to drive automated cutting machines, laser projection systems, fiber placement machines, and tape laying machines — and share it downstream and across the enterprise

Design for Additive Manufacture

Additive manufacturing is changing the way products are designed as well as how they are manufactured, by enabling optimized designs that were previously impossible or too expensive to make. Design, optimize, and build metal and plastic components using the latest additive manufacturing methods.

Design Interoperability

It’s no secret that products today are increasingly complex with many, if not most, reliant on integrated electronics. It is critical that designers of both systems collaborate throughout the development process in order to prevent conflicts and ensure alignment between each system prior to design completion.

Design Validation

Our products deliver visual product analytics and validation tools that enable you to quickly synthesize information, check designs for compliance to requirements, and make informed decisions.

Digital Mockup

Use real-time digital mockup tools to detect and resolve design issues using the product’s digital twin early in your product lifecycle. Teamcenter visualization mockup capabilities enable you to create high-level digital prototypes comprised of thousands of parts. You can check interferences, conduct part motion studies, and determine whether sufficient accessibility is provided to facilitate maintenance procedures. You can distribute the universally viewable information to other team members to annotate concerns or incorporate alternative design concepts.

Czy zainteresowało Cię [[global-preference-center-interest-placeholder]]?

Subskrybuj najnowsze informacje o [[global-preference-center-interest-placeholder]]

Ojej.

Przepraszamy, ale dane rejestracyjne do nas nie dotarły. Spróbuj ponownie.

Dziękujemy za rejestrację! Subskrybujesz wiadomości po raz pierwszy? Sprawdź swoją skrzynkę e-mail — znajdziesz tam wiadomość, która pozwoli Ci potwierdzić subskrypcję.

To pole jest wymagane Należy podać prawidłowy adres e-mail
To pole jest wymagane Nieprawidłowa wartość lub zbyt wiele znaków
To pole jest wymagane Należy podać prawidłowy adres e-mail