Cooling

Enter the summary here - no longer than 75 - 150 words. Use two paragraphs if the text is over 75 words. This is the full version of the summary text which will appear on the full version of the solution page.
Enter the summary here - no longer than 75 - 150 words. Use two paragraphs if the text is over 75 words. This is the full version of the summary text which will appear on the full version of the solution page.

Learn More

Enter the details here - Long version of what this solution does. This is displayed on the solution page in the Learn More block.

Webinar na żądanie | 46 min.

High fidelity aerodynamic simulation for gas turbine design

Gas turbine design

Learn how Siemens Energy create high fidelity turbine simulations by combining results from different disciplines, to create efficient and reliable gas turbine designs.

Obejrzyj webinar

Możliwości rozwiązania

Explore the key areas of this solution.

Electrics

Benefit from off-the-shelves models for batteries, fuel cells, power converters, linear actuators and electric motors to build any kind of electrical device architecture. Using the Simcenter Amesim multi-physics, multi-level, scalable and flexible approach, you can address many engineering issues like the design of the thermal management system, the assessment of the system performance or efficiency with realistic mechanical or hydraulic loads, as well as the design and validation of your control.

Fluid dynamics simulation

Simcenter provides industry leading computational fluid dynamics software allows you to simulate almost any engineering problem that involves the flow of liquids, gases (or a combination of both), together with all of the associated physics.

Fluids

Assess the overall behavior of hydraulic or pneumatic systems and components. Simcenter Amesim comes with a set of predefined functional components for pumps, compressors, valves and actuators, as well as with a series of detailed geometry-based components. You can study the evolution of pressures, flow rates and temperatures in the complete system, and analyze the performance of specific components (valves or pumps), taking into account compressible flow, mixtures of gases, thermal effects, aeration and cavitation.

Multi-physics simulation

Complex industrial problems require solutions that span a multitude of physical phenomena, which often can only be solved using simulation techniques that cross several engineering disciplines.

Simcenter Engineering and Consulting

Accelerate product development and solve the toughest problems with scalable help from engineering and consulting services.

Thermal simulation

Simcenter includes comprehensive, best-in-class thermal simulation capabilities that can help you to understand the thermal characteristics of your product and subsequently tailor your thermal management solution for optimal performance.

Thermodynamics

Model any type of thermal management systems by simulating heat transfer between solids, liquids and gas as well as phase change phenomena with Simcenter Amesim. Benefit from a comprehensive set of components such as pumps, thermostats or heat exchangers to accurately study the transient behavior of your system. Simcenter Amesim enables you to size components and compare different architectures or control strategies while accounting for thermal interactions between different subsystems.

Czy zainteresowało Cię [[global-preference-center-interest-placeholder]]?

Subskrybuj najnowsze informacje o [[global-preference-center-interest-placeholder]]

Ojej.

Przepraszamy, ale dane rejestracyjne do nas nie dotarły. Spróbuj ponownie.

Dziękujemy za rejestrację! Subskrybujesz wiadomości po raz pierwszy? Sprawdź swoją skrzynkę e-mail — znajdziesz tam wiadomość, która pozwoli Ci potwierdzić subskrypcję.

To pole jest wymagane Należy podać prawidłowy adres e-mail
To pole jest wymagane Nieprawidłowa wartość lub zbyt wiele znaków
To pole jest wymagane Należy podać prawidłowy adres e-mail