Production Planning & Scheduling

Enter the summary here - no longer than 75 - 150 words. Use two paragraphs if the text is over 75 words. This is the full version of the summary text which will appear on the full version of the solution page.
Enter the summary here - no longer than 75 - 150 words. Use two paragraphs if the text is over 75 words. This is the full version of the summary text which will appear on the full version of the solution page.

Learn More

Enter the details here - Long version of what this solution does. This is displayed on the solution page in the Learn More block.

Możliwości rozwiązania

Explore the key areas of this solution.

Advanced Constraint Modeling (Professional)

Model advanced resource constraints, such as rules about concurrent rule usage, and advanced inter-operation constraints including limits on the time between operations and how much operation times can be extended.

Advanced Material Handling

Implement custom rules about how materials are consumed to ensure that sub-assemblies and raw materials are consumed according to business rules.  When allocating materials, the system filters and ranks data to allow quality-related or customer-specific material usage constraints to be accounted for.

Advanced Schedule Optimization (Professional)

Define additional schedule optimization rules to deal with problems such as minimizing changeover times, preferred sequencing and campaigning.  Composite rules can be built with the SIMATIC IT Preactor workflow tool.

Assembly Process Visualization (Professional)

Visualize the assembly process from raw materials through to finished goods and sales orders in the Material Explorer. This shows a graphical view of the material dependencies as well as plots of stock levels over time. See where shortages will occur and choose to keep them as a constraint, or ignore them.

BOM Level Planning

The planning Bill of Materials (BOM) can be exploded, and then the production plan for lower level items is calculated in the same way. Based on the MOM explosion and the production plan, proposed material purchase requirements can be exported to an ERP system or Excel for action.

Development Environment (Ultimate)

Gives access to the full flexibility possible. Database schema and constraint model can be altered as required, including adding tables and fields. Create custom scheduling rules to solve specific scheduling problems and custom data manipulation tools for use with the workflow engine.

Interactive Schedule Viewing (Ultimate Viewer)

Allows interaction with the schedule, but changes cannot be saved.  Viewers can be used in the sales office to track the progress of orders and carry out order inquiries against a read-only copy of the published schedule. Management can use them to compare actual times with scheduled completion times to assess performance of the production process. Viewers can be used on a shop floor PC to provide the cell supervisor or machine operator with up-to-the-minute work-to-lists generated by the scheduling system.

Interactive Schedule Visualization

Once an initial Master Production Schedule (MPS) has been created, data can be displayed as stock profile graphs and capacity usage graphs. The MPS can be changed by simply clicking and dragging a point on the stock or capacity graphs, and the production of a particular item can be moved from one planning period to another. Any changes made will be reflected in all the linked plot and grid windows.

Make-To-Order Planning

In a make-to-order environment, stock levels of finished and intermediate items will not be part of the key process parameters. But there will still be the need to evaluate the effects of future demand changes on the manufacturing process. When a change in demand occurs, whether in terms of quantity or delivery dates, there is a need to be able to quickly assess if it is possible to meet the new requirements.

Czy zainteresowało Cię [[global-preference-center-interest-placeholder]]?

Subskrybuj najnowsze informacje o [[global-preference-center-interest-placeholder]]

Ojej.

Przepraszamy, ale dane rejestracyjne do nas nie dotarły. Spróbuj ponownie.

Dziękujemy za rejestrację! Subskrybujesz wiadomości po raz pierwszy? Sprawdź swoją skrzynkę e-mail — znajdziesz tam wiadomość, która pozwoli Ci potwierdzić subskrypcję.

To pole jest wymagane Należy podać prawidłowy adres e-mail
To pole jest wymagane Nieprawidłowa wartość lub zbyt wiele znaków
To pole jest wymagane Należy podać prawidłowy adres e-mail