Thermo-Mechanical Performance Engineering

Enter the summary here - no longer than 75 - 150 words. Use two paragraphs if the text is over 75 words. This is the full version of the summary text which will appear on the full version of the solution page.
Enter the summary here - no longer than 75 - 150 words. Use two paragraphs if the text is over 75 words. This is the full version of the summary text which will appear on the full version of the solution page.

Learn More

Enter the details here - Long version of what this solution does. This is displayed on the solution page in the Learn More block.

Możliwości rozwiązania

Explore the key areas of this solution.

Composites

In the quest to make products lighter yet stronger, manufacturers are increasing their use of composite materials. Simcenter is at the leading-edge of composites analysis through continuous development of material models and element types. Simcenter speeds the entire process for simulating laminate composite materials through a seamless connection to composites design, accurate solvers, and comprehensive post-processing.

Design Exploration

Design exploration software takes simulation to the next level by allowing users to determine appropriate values of variables that yield product designs that result in exceptional performance

Design for Additive Manufacture

Additive manufacturing is changing the way products are designed as well as how they are manufactured, by enabling optimized designs that were previously impossible or too expensive to make. Design, optimize, and build metal and plastic components using the latest additive manufacturing methods.

Motion Simulation

Understanding the operating environments for intricate mechanical systems – like in photocopiers, sliding sunroofs, or wing flaps – can be challenging. Motion simulation calculates the reaction forces, torques, velocities, acceleration and more for mechanical systems. You can directly convert CAD geometry and assembly constraints into an accurate motion model or create your own motion model from scratch, and the embedded motion solver and robust post-processing capabilities allow you to study of a broad range of product behaviors.

Process & Data Management

Enter the short summary here - no longer than 75 words. This is the version of the summary that will appear when this Capability is used in a promotion format.

Simcenter Engineering and Consulting

Accelerate product development and solve the toughest problems with scalable help from engineering and consulting services.

Structural simulation

Understanding how a component or product assembly reacts under stress or vibration is critical in any industry, but as products and materials become increasingly complex, engineers need tools that go beyond linear statics analyses. Simcenter includes the structural solutions you need for a wide range of structural analysis problems within a single user environment.

Thermal simulation

Simcenter includes comprehensive, best-in-class thermal simulation capabilities that can help you to understand the thermal characteristics of your product and subsequently tailor your thermal management solution for optimal performance.