새로운 프로그램을 위한 혁신적이며, 협업이 가능한 동기화된 프로그램 관리
Our products enable a wholistic engineering of production systems from mechanical concept through to complete PLC code. Discover a whole new level of collaboration with a toolset that enables a complete machine and plant design workflow, providing the highest level of design quality in the shortest time possible. Automation Designer offers a one-of-a-kind engineering toolset, designed from the ground up to enable controls engineers to complete their work with the highest efficiency, quality and speed possible.
Electrical and automation engineers work on the same backbone, with an integrated data model, saving time and eliminating errors. Directly integrate mechanical engineering data and receive updates, improving collaboration across your organization. Our integrated system also improves the quality of engineering results, while increasing efficiency by combining mechatronic models of existing designs and rule-based engineering to eliminate non-value added work. This, combined with our NX virtual commissioning capabilities, makes the complete process from concept to reality faster than ever before.
Our products enable a wholistic engineering of production systems from mechanical concept through to complete PLC code. Discover a whole new level of collaboration with a toolset that enables a complete machine and plant design workflow, providing the highest level of design quality in the shortest time possible. Automation Designer offers a one-of-a-kind engineering toolset, designed from the ground up to enable controls engineers to complete their work with the highest efficiency, quality and speed possible.
Electrical and automation engineers work on the same backbone, with an integrated data model, saving time and eliminating errors. Directly integrate mechanical engineering data and receive updates, improving collaboration across your organization. Our integrated system also improves the quality of engineering results, while increasing efficiency by combining mechatronic models of existing designs and rule-based engineering to eliminate non-value added work. This, combined with our NX virtual commissioning capabilities, makes the complete process from concept to reality faster than ever before.
Automation Designer allows for the direct integration of existing Siemens TIA Portal libraries and data. This allows for accelerated automation design.
Users of non-Siemens PLCs benefit from the export of signal and hardware information from the completed electrical design.
The central task of an electrical engineer is the design of electrical systems to bring the machine or line to life. With Automation Designer and it’s integration to EPLAN or through the NX Electrical Design Add-on, the electrical engineer can complete the design of the electrical system, while simultaneously completing the automation design.
Manual data transfer and double-work cause bottlenecks, slowdowns and unproductive time in a project. With a fully integrated electrical and automation data model, Automation Designer enables single engineering workflows that complete the work of multiple disciplines simultaneously. This increases efficiency and eliminates non-value added double work.
Integrate mechanical designs directly into your work through a common data backbone.
Standardization of engineering designs within single disciplines has brought improvements in the speed which new designs are created but is limited to incremental improvements of single disciplines. The ability to create mechatronic templates enables a new level of standardization, which significantly reduces engineering efforts and maintains unparalleled consistency of the entire design. It enables library objects that span design data from multiple disciplines.
Collaboration between disciplines is one of the most difficult and costly issues faced by machine and line builders today. Automation Designer addresses this issue by enabling mechanical, electrical and automation designers to simultaneously review, discuss and collaborate on their design. This breaks down barriers in the design process and helps teams collaborate more effectively and execute projects more efficiently.
The quality of engineering designs often suffers from errors caused in non-value added, repetitive activities. These actions, such as the definition of reference designations and symbolic names or even the creation of software or schematics can be automated through your design rules. This allows engineers to reduce errors and gives them more time to focus on creating value and driving innovation.
기능적, 메카트로닉 설계는 모델 기반 기능 정의와 더불어 Automation Designer에서 새로운 의미를 갖습니다.