새로운 프로그램을 위한 혁신적이며, 협업이 가능한 동기화된 프로그램 관리
Many of the new technologies that are disrupting heavy equipment industries, including innovative digital capabilities and electrification, lead to greater interactions between mechanical design, electronical and electronic systems design, and software. To achieve business success, manufacturers must find an effective way to deal with such multidisciplinary equipment design. But often, the way their organization grew over time, led them to have many disconnected teams, working in silos. Because of the complexity of multidisciplinary equipment design, this will result in endless iterations.
Siemens helps heavy equipment manufacturers accomplish complex multidisciplinary equipment design much faster by delivering an integrated and collaborative design environment where mechanical design, electronical and electric systems design, and software development can happen simultaneously. By following such a multidisciplinary equipment design approach, heavy equipment manufacturers can have all stakeholders collaborate in common tools and workflows, so that they have access to comprehensive multidisciplinary models and shared data. This will help them effectively master the complexity of multidisciplinary equipment design.
Many of the new technologies that are disrupting heavy equipment industries, including innovative digital capabilities and electrification, lead to greater interactions between mechanical design, electronical and electronic systems design, and software. To achieve business success, manufacturers must find an effective way to deal with such multidisciplinary equipment design. But often, the way their organization grew over time, led them to have many disconnected teams, working in silos. Because of the complexity of multidisciplinary equipment design, this will result in endless iterations.
Siemens helps heavy equipment manufacturers accomplish complex multidisciplinary equipment design much faster by delivering an integrated and collaborative design environment where mechanical design, electronical and electric systems design, and software development can happen simultaneously. By following such a multidisciplinary equipment design approach, heavy equipment manufacturers can have all stakeholders collaborate in common tools and workflows, so that they have access to comprehensive multidisciplinary models and shared data. This will help them effectively master the complexity of multidisciplinary equipment design.
As the teams for mechanical design, electrical and electronics systems design, and software development have so many interdependencies, their activities should not happen in separate tracks. Unfortunately, at many OEMs, this is the case, as a result of the way their organization evolved over time. Various departments are responsible for different disciplines and use disconnected tools and methods. Data exchange often happens via manual processes that are error-prone. To avoid that multidisciplinary equipment design will get stuck in endless iterations and rework, it is necessary to remove those silos by deploying an integrated environment that fosters collaboration between all multidisciplinary equipment design stakeholders, including other divisions if necessary and even suppliers. This collaboration can go from simply sharing their data to fully coupling their applications and will significantly speed up the overall multidisciplinary equipment design.
Multidisciplinary equipment design involves numerous parameters that interact. To master the complexity this entails, it is necessary to take control from the very beginning. Already during the concept phase, design teams must start with multidisciplinary analysis using comprehensive multidisciplinary equipment design models. Those won’t be perfect. But they will help to outline the boundaries for all the variables so that during all stages that come later in the process, there is a better starting point for optimization. As the design cycle moves on, the same models must be improved with up-to-date information and more details. This approach comes down to creating a digital twin for multidisciplinary equipment design - a virtual representation that mimics the product as good as possible in its current state, and that always stays in-sync. It is a single source of truth for all multidisciplinary design stakeholders.
Tactics like removing silos and building a digital twin will automatically unlock opportunities to frontload multidisciplinary equipment design decisions, or to shift left. That is important, because as the design process progresses, the opportunities to make changes become scarcer while to cost of implementing them explodes. This to a point where, depending on the magnitude of the required change, it could cancel the entire project. Via the digital twin, there is visibility on all decisions that are being taken by all design stakeholders. And also, when design stakeholders evaluate their decisions using comprehensive multidisciplinary models, they automatically take the wider context into consideration. Both will help to catch issues earlier. Besides, more frontloading can be achieved if silos are removed across departments. A good example is making CAE tools available through the CAD environment. In this way, analysts and occasional users get access to expert solutions, giving them the tools at hand to contribute to decisions that are otherwise taken at later stages.
오늘날 많은 제품들이 통합 전자 제품에 의존하고 있기 때문에 제품이 점점 더 복잡해지고 있다는 사실은 누구나 알고 있습니다. 충돌을 방지하고 설계 완료 전에 각 시스템 간의 조율을 보장하려면 개발 프로세스 전반에 걸쳐 두 시스템의 설계자가 협업을 수행하는 것이 매우 중요합니다.
Siemens 제품은 사용자가 신속하게 정보를 통합하여, 설계의 요구 사항 준수를 확인하고, 정보에 입각한 결정을 내릴 수 있도록 시각적 제품 해석 및 검증 툴을 제공합니다.
데이터를 관리하고 프로세스를 제어하며 통합을 사용해 포괄적 개발 흐름을 제공합니다. 제품 개발 프로세스 내에서 모든 주요 MCAD 및 PLM 툴을 사용해 도메인 간 변경 및 구성을 관리합니다.
비용, 무게 및 대역폭과 같은 목표에 대한 전기 및 전자 (E/E) 아키텍처를 최적화합니다. 기능을 정의하고 통합합니다. 전기, 전자, 임베디드 소프트웨어, 네트워크 사양을 생성하고 해석합니다.
Siemens 제품은 기업이 제품 설계를 가속화하고 비용을 절감할 수 있게 하는 포괄적인 지식 재사용 솔루션을 제공합니다. Siemens 솔루션은 제품 지식을 반복하여 활용할 수 있도록 지원함으로써 제품 지식의 가치를 극대화합니다.
보다 낮은 비용으로 보다 큰 혁신과 높은 품질을 제공합니다. Siemens PLM Software의 NX 제품 설계 소프트웨어는 설계 프로세스를 뛰어넘어 제품 개발의 모든 단계에 기능, 효율성 및 비용 절감을 제공합니다.
상세 타이밍 해석으로 '적절한 규모의' 통신 네트워크를 설계합니다. 네트워크 설계를 최적화하고 확인해 품질을 보장하고 개발을 가속화합니다. 정확한 통신 네트워크 구현을 제공합니다.
Teamcenter는 모든 MCAD (Mechanical Computer-Aided Design) 데이터를 단일 PDM (product data management) 환경에서 제공해 엔지니어링 생산성을 향상시킵니다. 사용하는 MCAD 툴 개수에 관계없이, 기본 MCAD 환경에서 다른 툴에서 생성한 부품과 어셈블리를 쉽게 찾고 수정해 다중 CAD 어셈블리 또는 제품 설계에 통합할 수 있습니다. 엔지니어링 변경, 검증 및 승인 프로세스를 자동화 해 사이클 타임을 단축하고 제품 품질을 향상시킬 수 있습니다.
Teamcenter 디지털 목업 및 시각화 기능을 사용하면 제품 라이프사이클 내 모든 관계자가 2D 및 3D 설계 데이터에 액세스하고 협업할 수 있어 정보에 기반해 제품 관련 의사결정을 내릴 수 있습니다. Teamcenter는 비용이 많이 드는 실제 시제품 대신 사용할 수 있는 가상 시제품을 여러 MCAD(Mechanical Computer-Aided Design) 형식에서 생성해 인체 공학 및 경로 계획 등과 같은 한층 특화된 스터디를 수행합니다. VR (가상 현실) 설계 검토 기능을 활용해 제품 디지털 트윈 가상 세계를 생생하게 체험할 수 있습니다.
Teamcenter 디지털 목업 및 시각화 기능을 사용하면 제품 라이프사이클 내 모든 관계자가 2D 및 3D 설계 데이터에 액세스하고 협업할 수 있어 정보에 기반해 제품 관련 의사결정을 내릴 수 있습니다. Teamcenter는 비용이 많이 드는 실제 시제품 대신 사용할 수 있는 가상 시제품을 여러 MCAD(Mechanical Computer-Aided Design) 형식에서 생성해 인체 공학 및 경로 계획 등과 같은 한층 특화된 스터디를 수행합니다. VR (가상 현실) 설계 검토 기능을 활용해 제품 디지털 트윈 가상 세계를 생생하게 체험할 수 있습니다.