Custom Equipment Design

equipment ready for delivery

Heavy equipment manufacturers get ever more requests for specialized custom equipment design. Across industries, companies are trying out innovative techniques, targeting new levels of productivity, sustainability, safety, and more. This often requires specialized machinery. Besides, as those companies are operating globally, they might need equipment that is suitable for specific local conditions or that is compliant with local regulations. Accommodating such individual requirements in a profitable way is challenging, especially as equipment is becoming increasingly complex.

Siemens helps heavy equipment manufacturers deliver all types of custom equipment design more efficiently by offering them an environment with modules for configure-to-order (CTO) design, engineer-to-order (ETO) design, or any combination in between. By using those solutions for CTO and ETO, heavy equipment manufacturers can build new configurations faster while maximizing commonality and reuse, speed up the development of new parts using automation, and improve collaboration and efficiency during verification and validation of numerous custom equipment design variants.

Heavy equipment manufacturers get ever more requests for specialized custom equipment design. Across industries, companies are trying out innovative techniques, targeting new levels of productivity, sustainability, safety, and more. This often requires specialized machinery. Besides, as those companies are operating globally, they might need equipment that is suitable for specific local conditions or that is compliant with local regulations. Accommodating such individual requirements in a profitable way is challenging, especially as equipment is becoming increasingly complex.

Siemens helps heavy equipment manufacturers deliver all types of custom equipment design more efficiently by offering them an environment with modules for configure-to-order (CTO) design, engineer-to-order (ETO) design, or any combination in between. By using those solutions for CTO and ETO, heavy equipment manufacturers can build new configurations faster while maximizing commonality and reuse, speed up the development of new parts using automation, and improve collaboration and efficiency during verification and validation of numerous custom equipment design variants.

custom equipment in operation

Learn More

Maximize commonality and reuse during custom equipment design

When offering custom equipment design, OEMs can achieve massive time and cost savings if they can maximize reuse of existing parts and components and if they optimize the commonality across the variants they have. To make this possible, their product planners must have access to data across all business lines and product segments as well as tools to leverage existing parts in building new configurations and validating those for compatibility. Those configuration-related choices should be made prior to and independent from the actual design process. And that single variability definition should then be maintained throughout the lifecycle. By doing so, decisions will be made for business reasons while everyone downstream in the process can focus on valid configurations using consistent data.

Enable any degree of custom equipment design

Offering customers more freedom of choice is commercially very interesting. But it adds pressure on the design team, as unique design requires dedicated engineering and because managing product data is more challenging if all serial numbers are different. A thorough digitalization of the design process is indispensable to achieve full custom equipment design or ETO. OEMs can save a massive amount of time if they can automate a part of the engineering process. For example, if based on legacy data, they can set up a rules engine where customer requirements and their organization’s capabilities are coupled and from which they can automatically generate technical content. In most cases however, requests are neither ETO not CTO, but somewhere in between. For those cases, design engineers need tools that have both CTO and ETO solutions, and where one solution is driving the other. Then any degree of custom equipment design can be accomplished efficiently.

Gain efficiency and flexibility by improving collaboration between custom equipment design stakeholders

Especially when working on various configurations simultaneously, OEMs cannot afford to lose time redoing work because teams for different disciplines were using inconsistent data or doing double work because they are not fully aware of each other’s activities. Therefore, it’s important that all stakeholders in the custom equipment design process, including peripheral divisions and suppliers, are connected through a common platform, where they have access to the same up-to-date data, so they can smoothly collaborate. By deploying such a digital infrastructure, many activities will happen way more efficiently, including generating the Bill of Materials, CAD, simulation and more. Such a platform should also facilitate proper change management. Change is necessary to continuously improve equipment, but it may impact many product areas. Understanding ‘how’ is crucial to make informed decisions or to anticipate. To implement change effectively and safely, it is necessary to deploy a systematic approach that provides increased visibility and control, across the various teams that may be impacted.

custom equipment in operation
주요 고객 성공 사례

ZOOMLION

Using Teamcenter and NX helps construction machinery manufacturer operate at optimal efficiency across 12 business divisions

Using Teamcenter and NX helps construction machinery manufacturer operate at optimal efficiency across 12 business divisions

ZOOMLION employs Siemens Digital Industries Software solutions to reduce data preparation times by 66 percent for new product processes

자세한 내용 보기

솔루션 기능

BOM (Bill of Materials) 관리

Teamcenter는 조직 전반에 공통된 BOM 정보 소스를 제공해 제품을 파악할 수 있도록 지원합니다. 기본적인 BOM 관리가 필요한 경우 또는 더 높은 유연성과 확장성을 갖춘 첨단 BOM 관리 및 구성이 필요한 경우 등 언제나 한층 혁신적이고 다양한 제품에 대한 시장 요구를 충족하고 그 이상의 만족도를 제공할 수 있습니다.

Engineering Automation

Rulestream 및 Teamcenter에서 ETO(주문 후 설계) 기능을 사용하여 제품 및 프로세스 규칙을 자동화할 수 있습니다. 이 자동화 기능을 통해 조직에서 정한 구속조건을 충족하면서 새로운 요구 사항을 빠르고 정확하게 해결할 수 있습니다. 몇 주가 아닌 몇 분 만에 입찰 및 제조 패키지를 생성할 수 있습니다. Rulestream을 사용하여, 수익성을 계속 유지하면서 ETO(주문 후 설계) 제품에 대한 고객 요구 사항을 지원할 수 있습니다.

Flexible Product Line Engineering

수익성을 유지하면서 다양한 고객 요구 사항을 지원합니다. Teamcenter를 사용하면 도메인 및 라이프사이클 전반에서 가변성의 단일 정의가 가능해집니다. 제품 옵션이 설계 데이터와 종속되어 있지 않고 조직 전체에서 활용할 수 있도록 독립적으로 관리됩니다. 따라서 사용하기 쉬운 구성 데이터의 공통 소스를 제공합니다. 플래너는 시장에 내놓고자 하는 제품, 제품 라인 및 기능을 정의합니다. 엔지니어는 유효한 구성에 집중합니다. 제조 단계에서는 동일한 정의를 활용하는 BOP를 생성합니다.

Product Configuration Integrations

구성된 제품의 진정한 관리 및 자동화를 위해서는 여러 독립형 ETO(주문 후 설계) 시스템과 독립형 제품 구성 관리 도구 또는 시스템이 필요합니다. Siemens PLM은 Teamcenter 및 Rulestream 통합의 강점은 물론 다른 소프트웨어에서 제공되는 고유한 기능도 활용할 수 있는 통합 제품 구성 관리 솔루션을 제공합니다. Siemens 제품 구성 관리 솔루션은 현재 비즈니스를 실행하기 위해 이미 사용하고 있는 가장 강력한 도구 중 일부와 통합됩니다.