Compliant Equipment Design

Compliant equipment harvesting

Today’s equipment design is always under time pressure because of the continuously growing product complexity and the increasing demand for customization. Besides, globalization adds more challenges, such as working in distributed teams, with all sorts of suppliers, and being confronted with numerous local regulations that become increasingly stringent. It’s important for heavy equipment manufacturers to stay focused on what ultimately matters most: delivering compliant equipment of consistently high quality that exceeds the industry standard anywhere, every time.

Siemens helps heavy equipment manufacturers build a solid reputation in the market by providing them with all the components they need to achieve compliant equipment design excellence. By deploying those solutions, manufacturers can make sure that throughout the entire process, all stakeholders in equipment design stay continuously focused on the requirements. They can take a systematic approach to verification management, based on a common environment where all data is stored and kept up to date. And they preserve, at any time, a clear view of deliverables, status, risks, and opportunities, and traceability of all decisions across the program.

Today’s equipment design is always under time pressure because of the continuously growing product complexity and the increasing demand for customization. Besides, globalization adds more challenges, such as working in distributed teams, with all sorts of suppliers, and being confronted with numerous local regulations that become increasingly stringent. It’s important for heavy equipment manufacturers to stay focused on what ultimately matters most: delivering compliant equipment of consistently high quality that exceeds the industry standard anywhere, every time.

Siemens helps heavy equipment manufacturers build a solid reputation in the market by providing them with all the components they need to achieve compliant equipment design excellence. By deploying those solutions, manufacturers can make sure that throughout the entire process, all stakeholders in equipment design stay continuously focused on the requirements. They can take a systematic approach to verification management, based on a common environment where all data is stored and kept up to date. And they preserve, at any time, a clear view of deliverables, status, risks, and opportunities, and traceability of all decisions across the program.

Compliant excavator

Learn More

Manage requirements and confidently achieve compliant equipment

Today is all about emissions. But compliant equipment design is also about aspects like safety, ergonomics, noise, vibrations and more. Unfortunately, around the world, many local variants of regulations apply. For globally operating OEMs, managing those so that their product groups understand and implement them correctly, is challenging. To simplify the problem, it is important that they see the similarities and differences across regions, so that they can translate all regulations into a set that is more concise and easier to work with. This can help, for example, to set up processes for automated design to regulatory requirements. Still, keeping all stakeholders focused on the requirements must be a continuous effort to achieve compliant equipment design. Proper requirement management means they must be captured, shared, and maintained in an integrated repository that participates in standard product lifecycle management services. They must be linked to tasks and resources to drive priorities, for continuous verification and validation, and to study the impact and the risk of change.

Exceed industry standards for compliant equipment by following a systematic verification management approach

Industry standards provide a framework for a common understanding of what appropriate quality or good practice is. To strengthen their reputation and protect their brand, OEMs must adhere to all the methods, processes, requirements, and specifications defined in those standards, and must also be able to proof this. Being a global industrial player as well as a user of the technologies we sell, at Siemens we have embedded vast knowledge of standards and regulations as built-in features in our solutions. With Siemens solutions, OEMs can conduct, for example, ergonomics analysis, visibility studies, and many more during compliant equipment design. Still, it requires a continuous effort to verify if the equipment meets the prescribed standards. Therefore, it is also necessary to deploy a systematic approach to verification and validation, one where all stakeholders can access the same, common up-to-date data set, where they can communicate instantly on information like data, requirements, and status, and where the impact of all decisions can be tracked throughout the entire compliant equipment design cycle.

Be accountable and transparent and provide proof of delivering compliant equipment

The relationship between OEMs and their customers often strongly relies on trust. And with emerging technologies such as autonomous and connected capabilities, this will become even more important as an increasing number of responsibilities will come to the OEMs. In this context, it is crucial for them to be transparent. They must keep track of requirements throughout the lifecycle and document all decisions that are being taken along the way, including changes. They must follow such a systematic and traceable approach to program management so that they are able to provide proof points of good practice for compliant equipment design in case there is a litigation. In fact, it will benefit all stakeholders if program managers, team leaders and designers are connected via a common platform where they share up-to-date information. With execution and planning tied together, everyone has immediate access to what they need for their job. This fosters efficiency, provides a clear view of deliverables, status, risks, and opportunities, and allows traceability of decisions across the program.

Compliant excavator
주요 고객 성공 사례

Pöttinger

Leading manufacturer of agricultural machinery uses Teamcenter to meet diverse needs of its customers

Pöttinger enhances decision- making, reduces errors and improves hit rate with Siemens Digital Industries Software solution

자세한 내용 보기

솔루션 기능

BOM (Bill of Materials) 관리

Teamcenter는 조직 전반에 공통된 BOM 정보 소스를 제공해 제품을 파악할 수 있도록 지원합니다. 기본적인 BOM 관리가 필요한 경우 또는 더 높은 유연성과 확장성을 갖춘 첨단 BOM 관리 및 구성이 필요한 경우 등 언제나 한층 혁신적이고 다양한 제품에 대한 시장 요구를 충족하고 그 이상의 만족도를 제공할 수 있습니다.

Product Requirements Engineering

요구 사항의 가치는 파악하는 데 있는 것이 아니라 제품 개발 프로세스를 주도하는 데에 있습니다. Teamcenter는 다양한 다운스트림 기능/형상/제품 아키텍처에 요구 사항을 할당하며, 이 모두는 보고서, 문서 및 대시보드를 생성하여 요구 사항 프로세스를 관리하는 동안 이루어집니다. Microsoft Word 및 Excel을 포함한 비슷한 Microsoft Office 애플리케이션에서 직접 요구 사항을 생성, 보기 및 편집할 수 있습니다. 라이프사이클 통합 요구 사항을 통해 전체 제품 라이프사이클에서 "통합을 시작하고 유지"한 개발 프로세스를 지원할 수 있습니다.

메카니컬 설계 관리

Teamcenter는 모든 MCAD (Mechanical Computer-Aided Design) 데이터를 단일 PDM (product data management) 환경에서 제공해 엔지니어링 생산성을 향상시킵니다. 사용하는 MCAD 툴 개수에 관계없이, 기본 MCAD 환경에서 다른 툴에서 생성한 부품과 어셈블리를 쉽게 찾고 수정해 다중 CAD 어셈블리 또는 제품 설계에 통합할 수 있습니다. 엔지니어링 변경, 검증 및 승인 프로세스를 자동화 해 사이클 타임을 단축하고 제품 품질을 향상시킬 수 있습니다.

변경 관리 및 워크플로

Teamcenter를 사용하면 PLM 프로세스를 관리하고 추적하는 데 드는 비용과 수작업을 줄일 수 있습니다. 여러 분야에 걸친 변경 관리부터 간단한 설계 검토 실행, 품질 문제에 대한 원활한 대처에 이르기까지 알맞은 데이터로 알맞은 작업에 인력을 집중시켜 적시에 알맞은 의사 결정을 내릴 수 있습니다. 변경 실행 시 모든 이해 관계자가 변경하는 내용과 이로 인한 영향을 정확히 파악할 수 있습니다.

시각화, 디지털 목업 및 가상 현실

Teamcenter 디지털 목업 및 시각화 기능을 사용하면 제품 라이프사이클 내 모든 관계자가 2D 및 3D 설계 데이터에 액세스하고 협업할 수 있어 정보에 기반해 제품 관련 의사결정을 내릴 수 있습니다. Teamcenter는 비용이 많이 드는 실제 시제품 대신 사용할 수 있는 가상 시제품을 여러 MCAD(Mechanical Computer-Aided Design) 형식에서 생성해 인체 공학 및 경로 계획 등과 같은 한층 특화된 스터디를 수행합니다. VR (가상 현실) 설계 검토 기능을 활용해 제품 디지털 트윈 가상 세계를 생생하게 체험할 수 있습니다.