새로운 프로그램을 위한 혁신적이며, 협업이 가능한 동기화된 프로그램 관리
Drivability is at the center of attention of automotive OEMs when developing xEVs. Electric motors, generators, and power electronics strongly impact energy-efficiency and performance of the vehicle.
Siemens Digital Industries Software offers an integrated, multi-scale, and multi-physics electric motor modeling and testing platform together with engineering and consulting services to support the development of reliable and energy-efficient electric machines.
Drivability is at the center of attention of automotive OEMs when developing xEVs. Electric motors, generators, and power electronics strongly impact energy-efficiency and performance of the vehicle.
Siemens Digital Industries Software offers an integrated, multi-scale, and multi-physics electric motor modeling and testing platform together with engineering and consulting services to support the development of reliable and energy-efficient electric machines.
Developing competitive xEVs for mass markets is ranked highly on the agenda of automotive OEMs. The choice of technology, topology, material, control strategy, and cooling system have a significant impact on the performance, drivability and noise & vibration levels of e-machines. Being able to model different electric machine topologies and simulate their performances from the system to their highest fidelity levels in an integrated environment can reduce development time considerably and provide opportunities for innovation to meet market expectations.
Siemens Digital Industries Software offers electric motor design simulation and testing solutions together with engineering and consulting services to accelerate the design and engineering of e-motors by virtually exploring design variants and assessing multi-level performance. Our solutions range from analytical to high fidelity electromagnetics simulation, system-level simulation, and design optimization. Using our tools engineers can leverage fast magnetic circuits-based models as well as FEA-based simulations. That synergy can also be automated to develop a design workflow for rapid but accurate analysis of all-electric machine types including motors, generators, and their drives. Our solutions also enable the designer to consider the effects of power electronic component losses, control strategy, coupled EMAG-CFD based thermal management, and the noise, vibration, and harshness analysis of e-motors.
Take simulation to the next level by quickly predicting the outcome of design changes on your vehicle performance.
Benefit from efficient modeling workflows to support your engineering effort from architecture creation to integration, including detailed design.
Accurately predict the interactions between electric, magnetic and flow fields and facilitate successful designs of electric machines and their cooling.
Get support in addressing complex engineering challenges thanks to our engineering experts from around the globe who will transfer their technical knowledge.
Optimize rotating machinery NVH performance by acquiring and analyzing the impact of design on sound quality, (torsional) vibrations, and energy efficiency.
Understand thermal characteristics and behavior and heat transfers between components, and tailor your electric device thermal management systems and their control for optimal performance.
Design efficient and reliable systems by keeping the temperature of components within the optimal operating range, evacuating excess heat or reusing it to improve performance and efficiency
고급 다단계 모델링 방식을 적용해 전기 서브시스템이 제품 전체 성능에 미치는 영향을 가상으로 평가합니다. Simcenter는 컨셉트 설계에서 제어 검증에 이르는 전기 시스템의 성능 극대화를 지원합니다.
차량 전동화는 자동차 산업의 지속적인 발전을 주도하는 힘입니다. 전기 자동차를 신속하고 수익성 높은 방식으로 생산하는 동시에, 소비자가 원하는 수준으로 제조하는 것은 매우 어려운 과제입니다. Siemens는 전기 자동차를 위한 정밀하고 통합된 디지털 트윈을 제공하여 모든 자동차 분야의 난제를 해결합니다. Siemens의 동급 최고 솔루션은 자동차 제조사와 차량 전동화 공급망이 개발 시간을 단축하고 프로세스의 모든 단계에서 변경 사항에 쉽게 적응할 수 있는 고품질 솔루션을 제공할 수 있도록 지원합니다.
Professor Pillay from Concordia University explains how they use Simcenter MAGNET and Motorsolve for electrical machine design for renewable energy...
Prof. Boulet of McGill University explains how integrating Simcenter MAGNET and Simcenter Motorsolve allowed them to design the entire power train.
High stress on modern electrical machines, the need for compact powertrain structure and high performance requirements are driving increased usage ...
The content and complexity of E/E systems are experiencing another step change due to vehicle electrification. Due to falling battery prices, elect...