革新的でコラボラティブ、かつ連携した新規プログラムの管理
Heavy Equipment
Construction, mining, and agricultural heavy equipment manufacturers striving for superior performance
Explore Industry中堅・中小企業
Remove barriers and grow while maintaining your bottom line. We’re democratizing the most robust digital twins for your small and medium businesses.
Explore IndustrySiemens Digital Industries Software Early Fault Detection with Vanti
The cost of SMT defects increases significantly as PCBs progress through the various manufacturing processes. In some cases, when an issue is found far down the line as part of regular quality management processes, it is no longer reversible, resulting in the unit being sent to the scrap heap. In other cases, fixing an item at a late stage may be possible but too expensive. Beyond the direct costs of the wasted material, finding errors late in the production process affects line yield. A solution that enables issues to be found early on in the production line can improve the first-pass yield calculation, reduce costs and improve yield, resulting in high throughput and high ROI.
With the Valor-Vanti Predictive Analytics Solution, we shift left SMT defect prediction, predicting faulty units earlier in the process, and thus reduce the cost of error.
The solution works by analyzing historical test measurements to create an early detection AI model. By training the AI model on the first test iterations, the solution can predict in real-time which units are most likely to fail at a later stage of the manufacturing process. Using predictive analytics in manufacturing, the units can be removed from the production line early on and sent for rework. As a result, a lower percentage of products will be faulty in the latter stages of production, resulting in higher throughput and productivity with improved quality and less waste.
The Valor-Vanti Predictive Analytics Solution is available as an annual subscription plan per product line (SKU), according to data volume and required latency. For high-mix, high-volume sites, usage-based pricing may be applied. Contact your local representative for pricing information.
The cost of SMT defects increases significantly as PCBs progress through the various manufacturing processes. In some cases, when an issue is found far down the line as part of regular quality management processes, it is no longer reversible, resulting in the unit being sent to the scrap heap. In other cases, fixing an item at a late stage may be possible but too expensive. Beyond the direct costs of the wasted material, finding errors late in the production process affects line yield. A solution that enables issues to be found early on in the production line can improve the first-pass yield calculation, reduce costs and improve yield, resulting in high throughput and high ROI.
With the Valor-Vanti Predictive Analytics Solution, we shift left SMT defect prediction, predicting faulty units earlier in the process, and thus reduce the cost of error.
The solution works by analyzing historical test measurements to create an early detection AI model. By training the AI model on the first test iterations, the solution can predict in real-time which units are most likely to fail at a later stage of the manufacturing process. Using predictive analytics in manufacturing, the units can be removed from the production line early on and sent for rework. As a result, a lower percentage of products will be faulty in the latter stages of production, resulting in higher throughput and productivity with improved quality and less waste.
The Valor-Vanti Predictive Analytics Solution is available as an annual subscription plan per product line (SKU), according to data volume and required latency. For high-mix, high-volume sites, usage-based pricing may be applied. Contact your local representative for pricing information.
Valor Predictive Analytics Solutions focus on solving small problems in the production line, one step at a time. Utilizing machine learning and artificial intelligence improves yield, quality, and OEE, to solve efficiency challenges.
登録して組み込みソフトウェアの最新情報を入手
登録できませんでした。もう一度やり直してください。
ご登録ありがとうございます! 初めての登録ですか? メールをチェックして登録されたかどうか確認してください。