革新的でコラボラティブ、かつ連携した新規プログラムの管理
Heavy Equipment
Construction, mining, and agricultural heavy equipment manufacturers striving for superior performance
Explore Industry中堅・中小企業
Remove barriers and grow while maintaining your bottom line. We’re democratizing the most robust digital twins for your small and medium businesses.
Explore IndustrySiemens Digital Industries Software Dispatching Production for Semiconductor
Learn more about Opcenter Execution Semiconductor
ExploreWell executed production plans result in shorter cycle times, fewer change-overs, on-time deliveries and reduced demand on limited resources. Proper sequencing of manufacturing operations and work-in-progress (WIP) driven by intuitive task management makes it easy for operators to perform the right job at the right time.
The solution supports various factors like critical ratios, up and downstream effects, maintenance plans, (sub) equipment setup and process capabilities. Dispatching is considered both from lot and equipment perspective.
Well executed production plans result in shorter cycle times, fewer change-overs, on-time deliveries and reduced demand on limited resources. Proper sequencing of manufacturing operations and work-in-progress (WIP) driven by intuitive task management makes it easy for operators to perform the right job at the right time.
The solution supports various factors like critical ratios, up and downstream effects, maintenance plans, (sub) equipment setup and process capabilities. Dispatching is considered both from lot and equipment perspective.
This capability enables the management of complex production that requires a many-to-many relationship between lots and equipment.
Multilayer clustered and chambered equipment can be controlled and tracked. Controlling the clustered equipment includes product-specific rules that avoid misusage by the operator in scenarios where it is not allowed.
The process enrichment capability enables the linkage of production orders to workflows and thereby provides more precise sequencing of work based on automatic and manual tasks.
It Provides the ability to create ad hoc additions or modifications to running production orders by using supplementary specifications without the need to change base master data but with change management control. Elements like recipes, equipment to use, steps to skip or add and specific work instructions can be added or modified.
Equipment Dispatching functionality allows the operator to load the equipment with the right production lots. It provides the ability to plan equipment usage based on constraints such as capabilities, maintenance, and others.
Manage work order changes during production execution in case events occur on the factory floor or there are changes in local availability and current conditions. This capability enables work order changes via reprioritization, splitting/combining of work orders lots, spec overrides, alternate process flows, and quantity adjustments.
This capability provides work order sequencing and execution based on dispatching rules for lots, batches, and serial numbered units. It enables step-specific sequencing and dispatch rules allow for station-specific rules to be applied when needed.
Opcenter Execution Semiconductor (旧Camstar Semiconductor Suite) は、半導体のフロントエンドとバックエンドの両方のオペレーションに1つで対応できる標準化された製造実行システムです。
登録して組み込みソフトウェアの最新情報を入手
登録できませんでした。もう一度やり直してください。
ご登録ありがとうございます! 初めての登録ですか? メールをチェックして登録されたかどうか確認してください。