革新的でコラボラティブ、かつ連携した新規プログラムの管理
Simulation is playing an increasingly significant role in the development of medical devices, saving development costs by optimizing device performance and reliability, reducing benchtop tests and clinical trials, and helping to speed the regulatory approval process.
Developing increasingly complex medical devices requires increasingly capable tools for simulation and testing. Our deep portfolio of simulation and testing solutions allows medical device developers to generate digital evidence of device performance across a range of engineering disciplines, throughout the product life cycle.
Simulation is playing an increasingly significant role in the development of medical devices, saving development costs by optimizing device performance and reliability, reducing benchtop tests and clinical trials, and helping to speed the regulatory approval process.
Developing increasingly complex medical devices requires increasingly capable tools for simulation and testing. Our deep portfolio of simulation and testing solutions allows medical device developers to generate digital evidence of device performance across a range of engineering disciplines, throughout the product life cycle.
Life sciences special report
The life sciences sector is experiencing an unprecedented change in the way new medical devices and pharmaceuticals are developed. Leading medical companies have realized that investing in modeling and simulation is critical, and have started integrating simulation into clinical trials and applying it to modernize their manufacturing processes. Ultimately, this results in better medicines, superior medical products, and significantly improved outcomes for patients. The articles in this special report highlight a few examples of this and cover a range of applications from medical device design to pharmaceutical manufacturing processes.
There has never been a greater opportunity to innovate in the design of medical devices, and to deal with the challenges of device development. Simulation is playing a critical role in identifying and preventing design-related failures, which continues to be the leading cause of device recalls. Simulation can increase product performance, safety and reliability, especially when performed early in the design cycle. And with the continuing rise in the cost of clinical trials, simulation-based product development, and virtual prototyping are increasingly being recognized by the US FDA as tools capable of supplementing experimental testing and clinical trials, and facilitating regulatory approval. Medical device developers can use simulation to generate digital evidence of product performance, an effort supported by FDA and regulatory agencies worldwide.
Engineers need tools that enable them to develop the most complete understanding of the complex processes occurring in the devices they design and troubleshoot, levels of understanding far beyond that provided by experiments or basic engineering principles. These tools should also allow engineers to explore the design space to understand the complex non-linear relationships between the relevant variables, then use the knowledge to inform trade-off decisions and provide insight into how products respond to the effects of variability, all while maintaining records of the simulation results and providing traceability between requirements and engineering data.
Explore the key areas of this solution.
Solutions for assessing the impact of variability from multiple interacting sources on product performance.
Predict product performance at every stage of the product development process--from system simulation to detailed multiphysics simulations of specific components and processes.
The platform for integrating simulation and test data into the broader, comprehensive database that comprises the "single source of truth" for your device.
Learn how system simulation can be used early in the medical device design process to size and balance device attributes, and frontload the develop...
医療機器業界では、設計上の欠陥を理由とする機器のリコール率が何年にもわたって増加しています。こうしたなか多くの企業が、問題を解決するための手段としてシミュレーション技術に注目しはじめました。シミュレーションを使えば、徹底的な設計探索を迅速に行って、予期せぬ欠陥やリコールのリスクを最小限に抑える...
シミュレーションが次世代埋め込み型医療機器設計の鍵を握る
コンピューター支援エンジニアリング (CAE) を活用することにより、医療機器設計の信頼性を確保し、設計品質を向上しながら、工数を大幅に削減できます。エンジニアリング・シミュレーションは現在、世界中の規制当局、メーカー、サプライヤーで広く採用されています。その一例として、米国食品医薬品局 (F...