革新的でコラボラティブ、かつ同期姓を確保した新規プログラムの管理
海洋産業では、全体的なパフォーマンスに優れ、エネルギー効率と信頼性が高く、環境への負荷が少ない船舶をより短い生産サイクルタイムと、より低い総運用コストで開発するための大きな変革が起きています。
How do you operate as ONE organization when your company counts 37 distinct business units worldwide, each having developed their own set of procedures and processes, master data, and software applications? Dutch shipyard Royal IHC understood that to maintain efficient workflows, a superior customer service, and a competitive market position, they would need to evolve and become 'ONE IHC'. They embarked on an ambitious and challenging multi-year transformation project, choosing Siemens Digital Industries Software as their trusted partner.
To remain competitive in today’s uncertain shipbuilding market, shipyards must deliver bids that are both attractive and accurate. As the demand for high value-added vessels increases, so does the need to control the risks associated with more complex design and manufacturing processes so projects are delivered on time and on budget. To this end, having a fully planned, resourced and budgeted end-to-end project management solution that integrates cost, schedule and technical requirements has become critical.
Browse and explore solutions in this industry segment.
Enter the short summary here - no longer than 75 words. This is the version of the summary that will appear when this Solution is used in a promotion format.
排出ガス基準および規制がますます厳格になり、船舶の性能はあらゆる側面で改善を余儀なくされています。性能目標を達成するには、革新的な設計を短時間で効果的に提供できなければなりません。シーメンスのソリューションは、船舶設計のあらゆる側面を検証し、求められる設計基準を満たすだけでなく、それ以上の成果を上げられます。
This solution is crucial to designing, building and sustaining future fleets on time, on budget and on performance. Additionally, it is essential for shipyards that plan to provide through-life service and support, and for fleet operating staff who have similar responsibilities.
Shipyards can dramatically improve content creation and management of documentation across the product lifecycle by using PLM to integrate ship design and technical publication domains. Our solutions enable engineering design and technical publication groups to share information across system repositories, reuse content and automate common domain functions and processes.
Composite Engineering and Manufacturing enables marine engineers to develop complex marine structures for the most challenging applications, and ensures reasonable manufacturing efficiency and production yields. With this solution, shipyards can be confident that their marine composite structures meet requirements for strength, weight and durability. Additionally, the solution provides shipyards and marine service centers with capabilities to manufacture replacement composite structures.
Transform your shipyard into a seamlessly integrated and synchronized enterprise linking designers, engineers, production specialists, support teams, partners and suppliers to optimize performance, maximize lifecycle productivity and sustain competitiveness. Our holistic shipbuilding solution spans the entire shipbuilding enterprise and lifecycle to enable shipbuilders to integrate their organizational knowledge, automate processes throughout the product lifecycle and improve efficiency, accuracy and execution to reduce time-to-delivery.
Today’s ships are far more complex to design, build and maintain throughout their lifecycle than they ever were before. Our solutions accelerate the development of modern ships and offshore structures so you can better respond to today’s demand for more energy-efficient, reliable and environmentally friendly vessels with better overall performance and lower total operating costs. Reduce design time and improve quality of production with next-gen software for piping, equipment and systems design for ships and offshore structures.
Accelerate the development of modern ships and offshore structures to respond to today’s demand for more energy-efficient, reliable and environmentally friendly vessels with high performance and low total operating costs. Reduce design times and improve quality of production with a next-generation software for design of steel outfitting parts and all mechanical equipment, components and systems.
Accelerate ship and offshore structure development to respond to today’s demand for energy-efficient, reliable and environmental-friendly ships and offshore structures with high performance and low operating costs. Use the focused environment provided in our next-generation ship structure design software to model and manufacture complete ship structures.
The demand for sustainable ships is growing significantly. By ensuring that future classes of ships and the shipyards that design and build them are fully compliant with both current and future environmental requirements in all stages of a ship lifecycle, this solution will support your eco-design initiatives and help you minimize the risks and costs associated with noncompliance.
流体力学パフォーマンスエンジニアリングは、あらゆる船舶の設計最適化に欠かせません。シーメンスのソリューションを使用すると、実際の航行条件下における船舶の流体力学をフルスケールで解析できます。仮想の試験水槽を使って、船体抵抗、自航、操縦、船体加速、付属物の形状、配列など、流れやパフォーマンスに関するあらゆる検証を実行します。
燃料効率を向上させるには、エンジンとパワートレイン設計の総合的なアプローチが必要です。テストと高度なシミュレーション機能を統合したシーメンスの製品ポートフォリオを使用すると、エンジンの設計と統合をあらゆる側面から詳細に解析できます。
Sound structural integrity is critical for viable operation, crew and passengers’ safety and comfort, as well as minimal environmental impact. Our simulation and testing solutions can predict fatigue life and hotspots while optimizing a product for durability.
Propeller performance is the key for efficient conversion of generated power into thrust force. We provide all the necessary tools to analyze propulsion system performance, from the propeller in isolation to sub-systems and full system performance for complete power management. Predict propeller performance, cavitation, and erosion using our hydrodynamics simulation capabilities, then analyze noise and dynamic response, vibration and structural integrity with our powerful 3D tools.
船舶の空気力学的パフォーマンスを最適化することは、安全で効率的な航行だけでなく、乗客の快適さにも欠かせません。シーメンスのソリューションを使って、船体の上部構造の抵抗や風荷重を予測し、空気力学的な効率性を向上させます。マルチフィジックスのシミュレーションツールにより、クリティカルな状況を設計早期に評価し、排ガスやヘリポートの安全性を解析できます。
Ensuring efficient vessel performance requires integration and optimization of multiple complex systems. Our solutions allow designers to check system architecture impacts on the complete vessel performance before any physical development takes place. Simulate and validate components early in the design cycle, and accurately predict system performance.
今日の造船市場では、より環境に優しく、スマートで、ハイテクな船舶が求められています。造船企業が競争力を保つためには、スケジュール、予算、および品質を守って、船舶を提供することが必要です。弊社の統合された船舶設計とエンジニアリングソリューションによって、設計スパイラルの管理が可能になります。複合領域の設計データや、プロセス、ツールをすべて、統合された環境に集約することで、情報やコラボレーションのサイロが解消され、イノベーションが促進され、組織の生産性が向上します。
As the demand for high value-added vessels increases, so does the need to identify and mitigate the risks associated with more complex design and manufacturing processes. This need is compounded by the current climate of unpredictability and increased competition in the shipbuilding market. To remain competitive, a shipyard must deliver bids that are both attractive and accurate. To this end, having a fully planned, resourced, and budgeted end-to-end project management solution has become critical.
Displaying of solutions.
Enter the short summary here - no longer than 75 words. This is the version of the summary that will appear when this Solution is used in a promotion format.
排出ガス基準および規制がますます厳格になり、船舶の性能はあらゆる側面で改善を余儀なくされています。性能目標を達成するには、革新的な設計を短時間で効果的に提供できなければなりません。シーメンスのソリューションは、船舶設計のあらゆる側面を検証し、求められる設計基準を満たすだけでなく、それ以上の成果を上げられます。
Enter the short summary here - no longer than 75 words. This is the version of the summary that will appear when this Solution is used in a promotion format.
Ship construction is a complex and lengthy process that demands careful planning and timely decision-making. Plan, optimize and validate ship construction processes before building. Use a broad range of tools to streamline your process planning workflows, automate non-value-added planning tasks and validate the best shipbuilding plan. These tools facilitate process design and sequencing, production BOM and BOP management, time management, 3D shipyard layout and ergonomic analysis. Control ship and production lifecycles from process planning and detailed engineering to full production by connecting the entire value chain to realize the best production strategy.
The demand for sustainable ships is growing significantly. By ensuring that future classes of ships and the shipyards that design and build them are fully compliant with both current and future environmental requirements in all stages of a ship lifecycle, this solution will support your eco-design initiatives and help you minimize the risks and costs associated with noncompliance.
流体力学パフォーマンスエンジニアリングは、あらゆる船舶の設計最適化に欠かせません。シーメンスのソリューションを使用すると、実際の航行条件下における船舶の流体力学をフルスケールで解析できます。仮想の試験水槽を使って、船体抵抗、自航、操縦、船体加速、付属物の形状、配列など、流れやパフォーマンスに関するあらゆる検証を実行します。
燃料効率を向上させるには、エンジンとパワートレイン設計の総合的なアプローチが必要です。テストと高度なシミュレーション機能を統合したシーメンスの製品ポートフォリオを使用すると、エンジンの設計と統合をあらゆる側面から詳細に解析できます。
Sound structural integrity is critical for viable operation, crew and passengers’ safety and comfort, as well as minimal environmental impact. Our simulation and testing solutions can predict fatigue life and hotspots while optimizing a product for durability.
Propeller performance is the key for efficient conversion of generated power into thrust force. We provide all the necessary tools to analyze propulsion system performance, from the propeller in isolation to sub-systems and full system performance for complete power management. Predict propeller performance, cavitation, and erosion using our hydrodynamics simulation capabilities, then analyze noise and dynamic response, vibration and structural integrity with our powerful 3D tools.
船舶の空気力学的パフォーマンスを最適化することは、安全で効率的な航行だけでなく、乗客の快適さにも欠かせません。シーメンスのソリューションを使って、船体の上部構造の抵抗や風荷重を予測し、空気力学的な効率性を向上させます。マルチフィジックスのシミュレーションツールにより、クリティカルな状況を設計早期に評価し、排ガスやヘリポートの安全性を解析できます。
Ensuring efficient vessel performance requires integration and optimization of multiple complex systems. Our solutions allow designers to check system architecture impacts on the complete vessel performance before any physical development takes place. Simulate and validate components early in the design cycle, and accurately predict system performance.
今日の造船市場では、より環境に優しく、スマートで、ハイテクな船舶が求められています。造船企業が競争力を保つためには、スケジュール、予算、および品質を守って、船舶を提供することが必要です。弊社の統合された船舶設計とエンジニアリングソリューションによって、設計スパイラルの管理が可能になります。複合領域の設計データや、プロセス、ツールをすべて、統合された環境に集約することで、情報やコラボレーションのサイロが解消され、イノベーションが促進され、組織の生産性が向上します。
As the demand for high value-added vessels increases, so does the need to identify and mitigate the risks associated with more complex design and manufacturing processes. This need is compounded by the current climate of unpredictability and increased competition in the shipbuilding market. To remain competitive, a shipyard must deliver bids that are both attractive and accurate. To this end, having a fully planned, resourced, and budgeted end-to-end project management solution has become critical.
Displaying of solutions.
デジタライゼーションによって船舶設計の持続可能性目標を達成する方法を学びます。
シミュレーション駆動アプローチは、船舶設計にかかるコストと時間を削減します。確信を持って目標を達成するには、どのような方法があるでしょうか。 造船業界は絶えず船舶効率を改善し、排出量を削減するよう迫られています。造船企業や船主にとって目標を確実に達成するための唯一の戦略は、可能な限り高効率な船...
包括的なデジタル・ツインで船舶設計を効率化
Is the design spiral holding you back? The design and engineering phase is one of the most critical of any shipbuilding project. The phase typicall...