“Under the sea” is the third session in a series of three webinars featuring BAR Technologies’ work at the leading edge of maritime innovation.
BAR Technologies have worked for and alongside their client SubSea Craft to design, build and test one of the most innovative craft in decades: SubSea Craft’s revolutionary VICTA Class Diver Delivery Unit (DDU) provides a truly unique combination of range, speed, and stealth – delivering outstanding operational capability.
VICTA combines the characteristics of a Long-Range Insertion Craft with those of a
Diver Delivery Unit. It moves quickly and seamlessly from the surface to sub-surface, limiting exposure to a minimum and therefore reducing the risk of being detected. This transition, along with its performance in both domains, is enabled by an innovative fly-by-wire control system, making VICTA a generation ahead of other surface-submersible DDU’s.
VICTA’s impressive performance on the surface (c40kts and 250nm endurance) is matched by equally striking specification underwater where 4hrs endurance is sufficient to navigate 2 crew and 6 divers for 25nm.
Its compatibility with a standard ISO shipping container means that it can easily and discreetly be moved to an area of operation. Equally, it can be lifted within the cargo bay of a standard transport aircraft (i.e. Lockheed C-130 Hercules) or underslung from a heavy-lift helicopter (i.e. Boeing CH-47
Chinook).
With significant input from a Special Forces operator and SEAL Delivery Vehicle (SDV) pilot with over 28 years of surface and sub-surface operational experience, VICTA designs reflect the needs of the operator.
Chief Technology Officer
Simon Schofield è Chief Technology Officer di BAR Technologies. Ha partecipato a varie competizioni: Volvo Ocean Race, America's Cup e a diversi gran premi navali. Di recente, Simon è stato Head of Design and Engineering presso BAR Land Rover, una squadra britannica che partecipa all'America's Cup dal 2016.