Esplora il settoreSoluzioni per macchinari industriali e attrezzature pesanti
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
Siemens PLM Software, a leader in media and telecommunications software, delivers digital solutions for cutting-edge technology supporting complex products in a rapidly changing market.
Explore IndustryApparecchiature medicali e farmaceutica
"Innovazione di prodotto personalizzata" attraverso la digitalizzazione per soddisfare la domanda del mercato e ridurre i costi
Esplora il settoreSmall & Medium Business
Remove barriers and grow while maintaining your bottom line. We’re democratizing the most robust digital twins for your small and medium businesses.
Explore IndustrySiemens Digital Industries Software JT Open Program
Siemens Digital Industries Software JT Open Program
The JT Open Program was formed by Siemens PLM software in 2003 at the request of a small group of forward-thinking corporations that saw value in the use of a common 3D format. That format is JT. The program now has over 100 members, including fortune 500 corporations located around the world and leading Academic institutions.
JT Open Program achievements include the publication of the JT file format specification and the creation of the industry leading no charge JT viewer, JT2Go. The publication of the JT specification was the impetus for ISO acceptance of JT as IS 14306. JT Open Program members continue to work collaboratively to expand the use of JT throughout the industry to achieve cost savings an efficiencies realized through the adoption of standard 3D JT data.
The JT Open Program was formed by Siemens PLM software in 2003 at the request of a small group of forward-thinking corporations that saw value in the use of a common 3D format. That format is JT. The program now has over 100 members, including fortune 500 corporations located around the world and leading Academic institutions.
JT Open Program achievements include the publication of the JT file format specification and the creation of the industry leading no charge JT viewer, JT2Go. The publication of the JT specification was the impetus for ISO acceptance of JT as IS 14306. JT Open Program members continue to work collaboratively to expand the use of JT throughout the industry to achieve cost savings an efficiencies realized through the adoption of standard 3D JT data.
The JT Open Program is open to any corporation, software vendor or academic institution. Interested parties can join the program as an advocate for no charge or select a fee-based membership. Fee-based memberships include corporate, vendor or academic. Fee-based memberships include access to the JT Open Toolkit. Vendor members can utilize the JT Open Toolkit to create applications for resale. The Program is made up of two boards, an executive level Management Review Board (MRB) and the Technical Review Board (TRB) All members are eligible to participate in Technical Review Board activities. MRB participation is managed through a ballot process. The JT Open program does not require the commitment of resource for participation.
JT Open Program members that have selected fee-based memberships have access to the JT Open Toolkit. The JT Open Toolkit is a C++ application programming interface (API) that provides read/write access to all JT file format content including; product structure, meta data, attributes, LODs, PMI and precise XT B-Rep geometry. The JT Open Toolkit reads and writes ISO compliant JT files and all production versions of JT currently supported by Siemens PLM products. Included with the toolkit is the PLM XMK SDK and a PLM XML JT Adapter that reads and writes PLM XML schema compliant XML. In addition, the toolkit includes a Unity game engine plug-in for reading JT content dynamically into a unity session and the JT Utilities. The JT Utilities provide a series of command line utilities that can be used to support application development and JT reuse scenarios.
Technology Fact Sheet
JT Open Toolkit Free Trial
JT File Format Reference (V10.5)
JT Data Format Reference Patent Clarification Notice
Subscribe to PLM Components updates
Spiacenti, non è stato possibile acquisire i dati inviati. Riprovare.
Grazie per la registrazione. È la prima sottoscrizione? Assicurati di controllare l’e-mail per confermare la sottoscrizione.
La live chat è disponibile dal lunedì al venerdì, dalle 8:00 alle 19:00 CST (USA). Inviaci un messaggio e ti risponderemo al più presto.
Invia un messaggio1-800-498-5351
Dal lunedì al venerdì, ore 7:00 – 20:00 CST