Boston, Massachusetts, 08 September 2016

Siemens’ NX Delivers Next Breakthrough in Product Design with Convergent Modeling

  • New technology helps engineers design parts optimized for 3D printing
  • Accelerates design by reducing need for data conversion
  • Unique capability simplifies reverse engineering of scanned models

The latest version of Siemens’ NX™ software (NX 11) delivers the next big breakthrough in digital product development with Convergent Modeling, a brand new modeling paradigm which greatly simplifies the ability to work with geometry consisting of a combination of facets, surfaces and solids, without the need for time-consuming data conversion. Convergent Modeling, the first technology of its kind, will help engineers optimize part design for 3D printing, speed up the overall design process and make reverse engineering a far more common and efficient practice in product design. In addition, NX 11 includes multiple enhancements throughout the integrated computer-aided design, manufacturing and engineering (CAD/CAM/CAE) solution, such as next generation 3D CAE, powered by the newly announced Simcenter 3D software, and improved CAM productivity with tools like robotics machining and hybrid additive manufacturing to help improve productivity.

“Siemens continues to invest in our core products to deliver innovative functionality such as Convergent Modeling, which we believe will be a game changer for digital product design,” said Joe Bohman, vice president, Product Engineering Software, Siemens PLM Software. “We anticipate Convergent Modeling will be a critical tool for efficiently working with facet geometry. This new one-of-a-kind technology is expected to provide huge savings in time and cost and help eliminate the error-prone rework phase, common when working with scanned geometry. It also removes the limitations associated with traditional CAD modeling when it comes to optimizing parts for 3D printing.NX11 simplifies the design process and supports the evolution of additive manufacturing to help companies realize a whole new level of creativity in product development.”

Product design is partially based on available materials and manufacturing approaches. New techniques like additive manufacturing open the door to create designs with forms and shapes that can provide higher levels of performance. Of course, traditional CAD technologies are built to support traditional manufacturing methods and have limitations when trying to optimize designs for additive manufacturing. Convergent Modeling removes these limitations by giving designers the flexibility to rapidly create new optimal shapes leveraging the materials and techniques made available through additive manufacturing.

Similarly, Convergent Modeling simplifies the process of working with scanned data. Users in various industries, including medical, auto and consumer goods, among others, are increasingly using scanned 3D data as part of the design process. This reverse engineering of existing designs has traditionally been an expensive and tedious process because the scanned data requires a time-consuming manual conversion of the faceted geometry into surface and solid form before it can be used for further modeling. Irregular shapes, in particular, require extensive rework so that they can be used for 3D printing, mold design, analysis, or other uses. The reverse engineering process can take days or weeks to complete. Convergent Modeling greatly reduces the need for this rework by bringing the scanned data in as facets that can be worked directly in NX 11, so there is no need to map surfaces, create solids, or do any other manual shape creation.

Convergent Modelling allows users to immediately begin using scanned data to create molds based on the shape, include it in an assembly, analyze it, or perform any other normal CAD operation. This, combined with the new 3D Print function in NX11 that enables users to 3D print designs directly from NX, significantly simplifies the additive manufacturing process. This new breakthrough scan, edit and print workflow uses the new Microsoft 3D print capabilities and supports the 3MF format to help ensure wide compatibility.

NX 11 also includes several other significant enhancements. Simcenter 3D now powers all simulation capabilities in NX for predicting product performance. Simcenter 3D, which is also available as a standalone application, provides NX users with a seamless experience as they move between design and simulation tasks. It speeds the simulation process by combining best-in-class geometry editing, associative simulation modeling and multi-discipline solutions embedded with industry expertise. Fast and accurate solvers power structural, acoustics, flow, thermal, motion, and composites analysis, as well as optimization and multi-physics simulation. For NX 11, Simcenter 3D introduces new capabilities for modeling and simulation of rotating machinery, a new environment for interior and exterior acoustics, and significant enhancements in damage analysis of composite structures.

Advanced technologies in NX 11 for manufacturing will help manufacturers expand machining flexibility and accuracy, reduce programming time, and improve part quality. New robotic programming capabilities in NX CAM extend the range of machining applications on the shop floor, enabling precise machining of large and complex parts using six-plus axis robots. Robotic machining automates manual operations, including polishing and deburring, improving repeatability to help deliver high quality parts. In addition, the enhanced feature-recognition capability automates NC programming of parts with many holes, to reduce programming time by up to 60 percent. NX CMM Inspection Programming’s new high-speed cycle takes measurements by moving only the head, rather than the CMM linear axes. The new head-touches method improves accuracy and speeds up inspection cycles by up to three times.

For more information please visit www.siemens.com/plm/nx11

Siemens PLM Software, a business unit of the Siemens Digital Factory Division, is a leading global provider of product lifecycle management (PLM) and manufacturing operations management (MOM) software, systems and services with over 15 million licensed seats and more than 140,000 customers worldwide. Headquartered in Plano, Texas, Siemens PLM Software works collaboratively with its customers to provide industry software solutions that help companies everywhere achieve a sustainable competitive advantage by making real the innovations that matter. For more information on Siemens PLM Software products and services, visit www.siemens.com/plm.

Follow us on Twitter at www.twitter.com/SiemensPLM

Siemens PLM Software, a business unit of the Siemens Digital Factory Division, is a leading global provider of product lifecycle management (PLM) and manufacturing operations management (MOM) software, systems and services with over 15 million licensed seats and more than 140,000 customers worldwide. Headquartered in Plano, Texas, Siemens PLM Software works collaboratively with its customers to provide industry software solutions that help companies everywhere achieve a sustainable competitive advantage by making real the innovations that matter. For more information on Siemens PLM Software products and services, visit www.siemens.com/plm.

Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is No. 1 in offshore wind turbine construction, a leading supplier of gas and steam turbines for power generation, a major provider of power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2015, which ended on September 30, 2015, Siemens generated revenue of €75.6 billion and net income of €7.4 billion. At the end of September 2015, the company had around 348,000 employees worldwide. Further information is available on the Internet at www.siemens.com.

Note: Siemens and the Siemens logo are registered trademarks of Siemens AG. NX and Simcenter are trademarks or registered trademarks of Siemens Product Lifecycle Management Software Inc. or its subsidiaries in the United States and in other countries. Microsoft is a registered trademark of Microsoft Corporation. All other trademarks, registered trademarks or service marks belong to their respective holders.

Contatto principale

Salim Rahimi
+1 972 987 3206
salim.hahimi@siemens.com

Come possiamo aiutarti?