Innovation et gestion de programmes synchronisée et collaborative pour les nouveaux programmes
Prove the safety and reliability of autonomous systems by using a leading physics-based simulation platform that allows for robust testing of autonomous vehicle functionality. Simcenter allows engineers to test, develop, and optimize autonomous systems by following a systematic approach. This will boost the overall systems engineering productivity from early research and development until the final stages of validation, certification, and homologation of autonomous vehicles.
Simcenter includes ready to use scenario libraries for various ADAS & AV functions and certification tests, combined with an extensive set of sensor models that allow for rapid assessment of every part of the complete full self-driving stack. It is an open environment that follows all the major industry standards and allows for integration with third-party tools and internal enterprise processes. Engineers can easily perform self-driving studies to determine the optimal sensor configuration for vehicles, develop robust driving assistance systems, evaluate the performance of perception, fusion, planning and control algorithms, and prepare for doing validation and certification of autonomous vehicle systems.
Prove the safety and reliability of autonomous systems by using a leading physics-based simulation platform that allows for robust testing of autonomous vehicle functionality. Simcenter allows engineers to test, develop, and optimize autonomous systems by following a systematic approach. This will boost the overall systems engineering productivity from early research and development until the final stages of validation, certification, and homologation of autonomous vehicles.
Simcenter includes ready to use scenario libraries for various ADAS & AV functions and certification tests, combined with an extensive set of sensor models that allow for rapid assessment of every part of the complete full self-driving stack. It is an open environment that follows all the major industry standards and allows for integration with third-party tools and internal enterprise processes. Engineers can easily perform self-driving studies to determine the optimal sensor configuration for vehicles, develop robust driving assistance systems, evaluate the performance of perception, fusion, planning and control algorithms, and prepare for doing validation and certification of autonomous vehicle systems.
Leverage a set of test scenarios that are compliant with major industry standards. The compatible tests available and their corresponding norm are: ISO test protocol for Adaptive Cruise Control (ACC), Euro NCAP performance tests for Autonomous Emergency Braking System (AEBS), ADAC performance tests for AEBS, ISO test protocol for Lane Departure Warning (LDW), NHTSA test protocol for LDW, Euro NCAP performance tests for Traffic Sign Recognition (TSR), ISO test protocol for Lane Change Assist System (LCAS) and eValue test protocol for LCAS.
Run simulations at scale. To prepare automated vehicle functionalities for operation, simply driving millions of highway miles is not sufficient. Instead, the industry needs the ability to stress-test automated driving algorithms, not only under normal conditions, but especially in fringe cases. That is where cluster simulation comes into play. Cluster capabilities in Simcenter allow engineers to test millions of scenarios while varying simulation parameters like vehicle parameters, weather, sensor parameters and many more.
Design human-machine interface (HMI) systems and subsystems by putting a driver directly in the loop, and more effective verify and validate physical ECU hardware components. Simcenter can project generated images into a physical camera using a special projection box, or inject them in the physical sensor processing pipeline, allowing engineers to test different levels of the ECU or other device under evaluation. This helps them to rapidly prototype ECU firmware and explore complicated edge-cases in a cost-effective and time-efficient manner.
Execute the variation of parameters. even from a single PC, which is particularly interesting for R&D and validation of ADAS systems. Simcenter offers the possibility to access all objects in scenarios via the Data Model API. With this programming interface, engineers can vary parameters in experiments, allowing for example automation and fast iteration.
Leverage a huge database of roads, infrastructure components, actors, weather, and light sources, and replicate a wide range of test cases, from simple showcase scenarios for validation of sensors, algorithms or even sensor fusion systems, to real-world traffic scenarios, within minutes. That will dramatically speed up verification and validation of self-driving cars. In Simcenter, engineers can use the GUI to develop scenarios visually and manually or use an API to generate scenarios via programming. Simcenter also includes import functionalities to help generate realistic representations of roads, traffic behavior and pre-determined scenarios.
Directly include a wide variety of top-notch sensor models in your simulations during the development of automated vehicles. The Simcenter sensor portfolio fully supports the development needs of automotive sensor suppliers, R&D applications at OEMs and Tier 1 suppliers, and series development of next-generation automated vehicles. Sensor models can be found in four main categories: ideal or ground truth sensors, probabilistic sensor models, detailed sensor models, and physics-based sensor models.
Get scalable help by choosing one of our different types of hands-on training and support packages. Our dedicated engineers help you better understand the different tools and capabilities. Training and support will also increase adoption speed and give engineers in-depth knowledge about how to best apply Simcenter for their specific use-case. We also offer services for customers that have specific requests beyond the scope of our standard software packages. We closely collaborate with engineering services that have in-depth knowledge of all possible applications for automated vehicles, such as ADAS Hardware-in-the-loop projects, sensor modeling and validation services, and real-life safety benefit assessments (for example for Euro NCAP Advanced).
Find the keys to a successful transition towards autonomous vehicle development
There is a clear trend in the market for driverless automotive systems. With consumer demand changing, progressive levels of driving automation wil...
As disruptive innovations in the automotive industry continue to increase, automakers now focus on overcoming the challenges that autonomous vehicl...
L'industrie automobile est en pleine mutation. Les technologies numériques sont à l'origine de la demande de solutions de transport autonomes, et e...