Innovation et gestion de programmes synchronisée et collaborative pour les nouveaux programmes
Integrate ship outfitting with a complete set of advanced functions that manage equipment, distributors, and related auxiliary structure design and fabrication. FORAN Machinery & Outfitting continues the design process by incorporating all aspects of equipment, piping, HVAC ducting, and auxiliary structures into the same project-centric database used for the ship structure.
Integrate ship outfitting with a complete set of advanced functions that manage equipment, distributors, and related auxiliary structure design and fabrication. FORAN Machinery & Outfitting continues the design process by incorporating all aspects of equipment, piping, HVAC ducting, and auxiliary structures into the same project-centric database used for the ship structure.
Work with equipment, piping, ventilation, cable trays (space reservation), auxiliary structures, and line supports. Data integrity prevents multiple accesses to objects.
Piping and HVAC ducts can be routed interactively or using user predefined solutions. Design any type of foundation, ladder, grating, and handrail, plus pipe, duct, and cable tray supports.
Define pipe and instrumentation diagrams as part of the ship design, stored in the same database as the 3D model. A 2D environment contains the necessary functionality to handle the basic entities that make up the essential part of the diagrams (equipment, pipes, fittings, and instrumentation).
All data included in P&ID's is available when working in the 3D model, guaranteeing correspondence between the diagrams and the product, therefore facilitating the task of creating the as-built diagrams.
Outfitting production documents are highly automated, especially the pipe spool isometric sketches for fabrication and mounting. Both drawing types allow symbols, labels, dimensions, boxes, and paper formats, and are automatic. The fabrication drawings can export data to CNC files.
Pipes, HVAC ducts, auxiliary structures, supports, and corresponding hotworks can be added at any level of structure assembly, thus guaranteeing the pre-outfitting blocks and sections with the consequent savings in cost and delivery times.
The Outfitting Standards Library includes technological attributes and built-in geometries so that pipes, fittings, and equipment are recreated from vendor catalogs. The pipes and fittings are organized in specifications and contain the complete list of attributes such as material, nominal and secondary diameters, schedule, and nominal pressure connection types. Define any 3D model for equipment and fittings by means of geometric macros.
Assign electric properties to equipment and fittings for full-electric calculation and wiring.
Pipe and HVAC fitters can identify each of the holes that must be cut into any plate for a watertight or non-watertight penetration. Penetrations carry their own data and are stored in the database. At the same time, they undergo a strict workflow from the Outfitting (and Electrical) Department to the Structure Department. The penetrations pieces have their own representation and can be included in the drawings and exported to BOMs.