Innovación y gestión de programas colaborativa y sincronizada para nuevos programas
Sector aeroespacial y defensa
Innovación y gestión de programas colaborativa y sincronizada para nuevos programas
Conocer el sectorAutomotive & Transportation
Integration of mechanical, software and electronic systems technologies for vehicle systems
Conocer el sectorProductos de consumo y comercio minorista
Innovación de productos mediante una gestión eficaz de las formulaciones integradas, el embalaje y los procesos de fabricación
Conoce el sectorComponentes electrónicos y semiconductores
El nuevo proceso de desarrollo de productos aprovecha los datos para mejorar la calidad y la rentabilidad y reducir el tiempo y los costes de comercialización.
Conocer el sectorEnergía y Utilidades
Supply chain collaboration in design, construction, maintenance and retirement of mission-critical assets
Conocer el sectorHeavy Equipment
Construction, mining, and agricultural heavy equipment manufacturers striving for superior performance
Explore IndustryMaquinaria industrial y maquinaria pesada
Integration of manufacturing process planning with design and engineering for today’s machine complexity
Descubra el sectorInsurance & Financial
Visibility, compliance and accountability for insurance and financial industries
Explore IndustrySector naval
Innovación en la construcción naval para reducir de manera sostenible los costes de desarrollo de la flota futura.
Conocer el sectorMedia & Telecommunications
Siemens PLM Software, a leader in media and telecommunications software, delivers digital solutions for cutting-edge technology supporting complex products in a rapidly changing market.
Explore IndustryDispositivos médicos y productos farmacéuticos
Innovación de los productos personalizados mediante la digitalización para satisfacer las exigencias del mercado y reducir los costes.
Conocer el sectorSmall & Medium Business
Remove barriers and grow while maintaining your bottom line. We’re democratizing the most robust digital twins for your small and medium businesses.
Explore IndustryEnable CI/CD of ECU software
Enable CI/CD of ECU software
Streamline ECU software development
In today’s automotive world, as we are moving towards ‘software-defined vehicles,’ the main differentiating factor is the software. Inspired by smartphone industry, users are expecting the latest software for their cars by Over-The-Air (OTA) for new updated or improved features as well as fixed issues. To meet this challenge, software needs to be continuously delivered, which in turn needs to be continuously developed, deployed and tested. CI/CD can help teams to reach this goal.
In this on-demand webinar, you will learn:
The automotive industry is transforming. In general, products and software require many updates over their lifecycles, such as obligatory security updates, next generation features and OTA updates. These updates keep vehicles up-to-date and trustworthy, as cars become more connected to the Internet. Users also want the latest features and updates to their cars. This means that software needs to be continuously developed, deployed, validated and updated faster than ever before. Manufacturers must develop an agile way of working, create software factories and use continuous integration to keep up with software updates.
There are many advantages of using CI/CD, such as:
The typical CI/CD workflow begins in the planning phase, which is driven by new features or feedback from different parties. This phase is broken down into smaller tasks – code, build and test. Then, the CD workflow begins with deploying in-test or production vehicles, followed by testing in a real-world scenario. After, the software is monitored, and feedback is collected from users and fed back into planning.
With AUTOSAR, the CI/CD workflow operates differently. The code phase in the CI workflow is broken into two steps – configuration and generation. The configuration step is where users will configure basic software and software modules based on requirements. Later, this configuration step is used to generate a code, and the workflow continue as described above.
The ability to develop and validate ECU software at the same time is one of the advantages of using CI/CD. Learn more about the benefits of a CI workflow in the on-demand webinar.
In the automotive industry, there is an increasing amount of complexity in vehicle systems paired with continuous pressure on cost and timing of creating vehicles. Developers must meet growing software safety concerns and regulatory demands. Additional challenges include the late detection of errors in the integration and testing process, along with the reuse and integration of application functions.
To overcome these challenges, developers can implement AUTOSAR to streamline ECU software integration. With a guided user interface, AUTOSAR includes sophisticated configurations managed by generative development flow. AUTOSAR enables the development of software in a platform context, which frontloads the process. This results in a high-performance embedded platform software that is scalable, safe and secure.
Lakshmi Narayanan
Senior Technical Product Engineer, Siemens Digital Industries Software
Lakshmi Narayanan works as Senior Technical Product Engineer at Siemens. He works closely with customers to understand and provide on-site support and solutions. Generating ideas and new features into the product is his focus area.
Hola Bob (este nombre será reemplazado por el nombre real cuando tenga lugar la visita al sitio web)
Nos gustaría saber más sobre usted.
Se ha producido un error en el envío de la página. Por favor, vuelva a intentarlo.
¿Es la primera vez que se suscribe a los correos electrónicos de Siemens Digital Industries Software? Asegúrese de confirmar su suscripción en el correo electrónico que recibirá en breve.
Hola Bob (este nombre será reemplazado por el nombre real cuando tenga lugar la visita al sitio web)
Podrá acceder a este webinar durante 90 días. Pulse abajo para iniciar la visualización.
Streamline ECU software development
In today’s automotive world, as we are moving towards ‘software-defined vehicles,’ the main differentiating factor is the software. Inspired by smartphone industry, users are expecting the latest software for their cars by Over-The-Air (OTA) for new updated or improved features as well as fixed issues. To meet this challenge, software needs to be continuously delivered, which in turn needs to be continuously developed, deployed and tested. CI/CD can help teams to reach this goal.
In this on-demand webinar, you will learn:
The automotive industry is transforming. In general, products and software require many updates over their lifecycles, such as obligatory security updates, next generation features and OTA updates. These updates keep vehicles up-to-date and trustworthy, as cars become more connected to the Internet. Users also want the latest features and updates to their cars. This means that software needs to be continuously developed, deployed, validated and updated faster than ever before. Manufacturers must develop an agile way of working, create software factories and use continuous integration to keep up with software updates.
There are many advantages of using CI/CD, such as:
The typical CI/CD workflow begins in the planning phase, which is driven by new features or feedback from different parties. This phase is broken down into smaller tasks – code, build and test. Then, the CD workflow begins with deploying in-test or production vehicles, followed by testing in a real-world scenario. After, the software is monitored, and feedback is collected from users and fed back into planning.
With AUTOSAR, the CI/CD workflow operates differently. The code phase in the CI workflow is broken into two steps – configuration and generation. The configuration step is where users will configure basic software and software modules based on requirements. Later, this configuration step is used to generate a code, and the workflow continue as described above.
The ability to develop and validate ECU software at the same time is one of the advantages of using CI/CD. Learn more about the benefits of a CI workflow in the on-demand webinar.
In the automotive industry, there is an increasing amount of complexity in vehicle systems paired with continuous pressure on cost and timing of creating vehicles. Developers must meet growing software safety concerns and regulatory demands. Additional challenges include the late detection of errors in the integration and testing process, along with the reuse and integration of application functions.
To overcome these challenges, developers can implement AUTOSAR to streamline ECU software integration. With a guided user interface, AUTOSAR includes sophisticated configurations managed by generative development flow. AUTOSAR enables the development of software in a platform context, which frontloads the process. This results in a high-performance embedded platform software that is scalable, safe and secure.
Lakshmi Narayanan
Senior Technical Product Engineer, Siemens Digital Industries Software
Lakshmi Narayanan works as Senior Technical Product Engineer at Siemens. He works closely with customers to understand and provide on-site support and solutions. Generating ideas and new features into the product is his focus area.