Innovación y gestión de programas colaborativa y sincronizada para nuevos programas
Registre todo el proceso de la fabricación aditiva con las soluciones de gestión de datos de Siemens. Estas no solo incluyen los datos asociados con las geometrías de las piezas, sino los datos que abarcan toda la configuración de la bandeja de construcción y los parámetros de impresión. Las estrategias de construcción, el tratamiento posterior y los procedimientos de validación también forman parte de la fabricación aditiva. La gestión adecuada de estos datos constituye la clave para lograr un proceso de fabricación aditiva del sector repetible y de calidad. Con Teamcenter de Siemens, se logra una gestión sencilla e integral de los datos de proceso.
Producing additive manufactured parts at an industrial scale, especially in metal, requires numerous manufacturing processes and post processes that must be managed. Setup and preparation of the printer as well as post-print steps such as substrate separation, heat treatment, finishing, and inspection are all steps that must be tightly controlled.
Managing materials for the additive manufacturing process is another area where a tightly controlled process is mandatory. Counting the number of recycles and mixed powder batches is necessary for tracing the materials used in your printing operations. This traceability is important because you can't disassemble mixed powders and the amount of recycled powder used may affect the quality of the final print.
Protect your organization intellectual property through robust data security measures. Siemens has partnered with Identify3D to integrate their suite of tools for protection of additive manufacturing data. The ecosystem provided by Siemens and Identify3D provides for a secure digital container to move and modify additive manufacturing data through the digital workflow. All of the necessary elements are integrated into the Siemens product set from NX CAD/CAM through to the machine controllers.
See how Konecranes manages the product lifecycle of mass-produced to custom lift products by collaborating across domains and departments
Reach more people and processes for greater business performance.