Innovation and collaborative, synchronized program management for new programs
The tire is a complex and highly non-linear vehicle component that has a significant effect on the behavior of a vehicle. As the number of vehicle models on the market continues increasing, so does the number of possible use cases that need to be tested and validated. This fact, in combination with everlasting strive for reduced development times, calls for ever more simulation instead of physical vehicle testing.
Modelling tire performance requires a lot of expertise and specialization. For this purpose, Simcenter offers engineers scalable and customized solutions. The ultimate goal of Simcenter Tire is simulation to accurately represent tire forces and moments, so they can be propagated to various vehicle performance simulations.
More specifically, the Simcenter Tire simulation toolchain consists of the Simcenter MF-Tyre/MF-Swift tire model, the Simcenter MF-Tool tire model parameterization tool and tire testing services. The Simcenter MF-Tyre/MF-Swift model is available with all major vehicle dynamic simulation packages.
The tire is a complex and highly non-linear vehicle component that has a significant effect on the behavior of a vehicle. As the number of vehicle models on the market continues increasing, so does the number of possible use cases that need to be tested and validated. This fact, in combination with everlasting strive for reduced development times, calls for ever more simulation instead of physical vehicle testing.
Modelling tire performance requires a lot of expertise and specialization. For this purpose, Simcenter offers engineers scalable and customized solutions. The ultimate goal of Simcenter Tire is simulation to accurately represent tire forces and moments, so they can be propagated to various vehicle performance simulations.
More specifically, the Simcenter Tire simulation toolchain consists of the Simcenter MF-Tyre/MF-Swift tire model, the Simcenter MF-Tool tire model parameterization tool and tire testing services. The Simcenter MF-Tyre/MF-Swift model is available with all major vehicle dynamic simulation packages.
Analyze all vehicle dynamics using an all-in-one tire model. Simcenter MF-Swift extends MF-Tyre with turn slip modeling, tire belt dynamics and generic 3D obstacle enveloping for parking, ride comfort, road load prediction, and vibration analysis. The modular setup allows the model complexity to be adapted to the engineering problem. Simcenter MF-Swift is the fastest tire model on the market for 3D uneven road simulations. Thanks to its transparent structure, engineers can easily tune or estimate parameters during early development, when no physical tires are available. Its modeling functionalities have been developed and extensively validated using numerous measurements, experiments and customer use cases.
Accurately simulate steady-state and transient behavior up to 8Hz, for handling, control prototyping, and ADAS analyses. Simcenter MF-Tyre is the global standard implementation of the Pacejka Magic Formula, including the most recent modeling developments such as inflation pressure effects, estimated combined slip behavior and a non-linear representation of tire transient behavior. MF-Tyre is the only Magic-Formula-based tire model that is available in all major vehicle dynamic simulation packages, allowing in- and intercompany standardization.
Convert a Simcenter MF-Tyre/MF-Swift model into a real-time variant without model reduction, to guarantee equal numerical results across all stages. Over the course of the product development trajectory, various simulation environments pass by, including desktop applications, HiL setups, and driving simulators. Simcenter helps engineers use a standardized tire model across all simulations, by adapting the model to the required computational performance without affecting results. Consequently, Simcenter MF-Tyre/MF-Swift is currently supported on most industry-standard Real-Time operating systems.
Measure tire performance for many road surfaces, covering dry, wet, snow and icy road conditions, using an on-road test laboratory. The Simcenter test trailer is specifically designed to measure the forces and moments a tire yields when on the road in various situations. Both passenger car and motorcycle tires can be measured. On the in-house developed motorcycle tire measurement setup, tires can be measured at camber angles up to 70 degrees. Besides gathering the input for the Simcenter MF-Tool parameter identification tool and subsequently the Simcenter MF-Tyre/MF-Swift tire models, the measurement facilities are also used for validation and benchmarking studies.
Convert measured data into parameters for Simcenter MF-Tyre/MF-Swift models using a user-friendly tire parameter identification tool that includes data visualization, database functionality, and advanced estimation capabilities. The Simcenter MF-Tool also enables visualization and tuning/modification of tire models. It allows engineers to study the effects of changing tire conditions such as tire inflation pressure, stiffness, friction levels, by the automatic scaling of tire properties. Users can also create their own "virtual tire" by modifying tire properties with standard tire model parameters or measured data.
Collaborate with our engineers and achieve a highly accurate and efficient tire modeling process. Simcenter Engineering services experts provide scalable help, from testing on location to set up dedicated tire testing protocols. Project results can perfectly integrated into existing processes and can be complemented with training on the use of Simcenter MF-Tyre/MF-Swift. Other typical engineering services are tire testing protocol and parameter identification improvement and/or automation, tire test rig improvements, studies to the correlation between specific tire characteristics and vehicle dynamics performance criteria and in-depth transfer of tire performance knowledge.
Accurately represent tire behavior throughout the vehicle design process
Providing a versatile and cost-efficient approach to tire modeling
Fulfilling the vehicle dynamics simulation requirements from an automated driving perspective
Easily access high-quality tire model parameter sets for vehicle dynamics simulations