Innovation and collaborative, synchronized program management for new programs
Deliver greater innovation and higher quality at lower cost. With NX you can use the most productive modeling approaches interchangeably – from explicit solid and surface modeling to parametric and direct modeling, along with facet-based modeling.
Deliver greater innovation and higher quality at lower cost. With NX you can use the most productive modeling approaches interchangeably – from explicit solid and surface modeling to parametric and direct modeling, along with facet-based modeling.
30-day free trial. Start designing in minutes.
Start designing with your free trial of NX Cloud Connected Products and learn how you can develop world-class products using powerful NX CAD capabilities. NX Cloud Connected Products deliver the high-performance design capabilities of NX, the leading solution for product design. Our free, online trial lets you try any of our NX Cloud Connected Products before you buy. No installation required; start designing in minutes.
NX users have a range of visualization modes that can be used to display an appropriate Visual Twin of their data as it moves along the Digital Thread matching their workflow with full associativity. Users can easily switch between these visualization modes at the click of a button to ensure an optimized balance between speed, quality and performance.
NX Virtual Reality enables NX users to review their designs at human scale, giving you the ability to get up close and personal with full size models. NX Virtual Reality is integrated into the desktop application and accessible with one click, extending familiar interactions into a truly immersive 3D environment. Secure, multi-user sessions, facilitate collaboration across a whole range of key stakeholders, resulting in better design understanding and communication throughout the product development process.
NX offers an expert personal assistant that uses Artificial Intelligence and Machine Learning to track and learn from user actions. It then predicts the NX commands the user will likely use next based on the context of what they are currently doing and then presents those commands on a compact adaptive UI panel. For example, if you’re doing something in sheet metal, it knows that a certain sequence of commands are being used within sheet metal, or tool design, or casting design… It then starts presenting commands to you that it thinks you’re going to use next. It actually understands that there is a sequence.
Convergent modeling technology in NX gives anyone the ability to perform faceted-based modeling without the need for data conversion. By combining facet, surface and solid modeling in a single integrated environment, NX eliminates the need for reverse engineering. Simply model with topology optimization results directly. Convergent Modeling, compared with traditional modeling techniques, is 10 times faster.
Certain functional surfaces and solids are most easily defined using mathematical equations. Functional examples include optical surfaces, cam profiles, airfoil geometry, and any other geometry for which you can define the math. Equation-driven geometry can be defined using robust 3D plotting tools in NX Maple and then associatively incorporated into NX designs for further refinement, using Convergent Modeling. NX Maple can easily handle algebraic math, differential and integral calculus, differential equations, linear algebra, and much more. You’ll have final control over the smoothness or resolution of equation-driven geometry created by NX Maple. And the intellectual property defined by NX Maple worksheets can easily remain managed within Teamcenter.
NX Token licensing provides a very flexible and cost-effective way for customers to run almost any NX Product Engineering add-on module. This results in increased cost savings for customers who will run a wide variety of applications on an occasional basis.
Modeling is amazingly fast and intuitive with NX – you have the freedom to modify 3D geometry without understanding how models were constructed using simple push-and-pull methods. For greater versatility, you can use synchronous modeling interchangeably with all other CAD modeling tools – on NX models or geometry from any other source.
Create and optimize a new generation of products by taking performance requirements into account from the start. Compressed schedules often force engineers to choose the first feasible design option. By mimicking nature’s evolutionary approach, generative engineering empowers you to identify the best design sooner while reducing the number of iterations needed.
Automated calculations iterate until optimized geometry is achieved. The resulting organic shapes are lightweight and meet all performance requirements. NX also uses HEEDS® multidisciplinary design exploration software to automate the design exploration process.
From concept design through engineering and manufacturing, NX gives you an integrated toolset that coordinates disciplines, preserves data integrity and design intent, and streamlines the entire process.
NX is available via perpetual licensing, subscription, and rental options. Deployment options include on-premise, or a virtualized environment or a streamed service from a public cloud provider. Rather than a large up-front investment in a perpetual license, Cloud Connected Products provide the option to purchase an annual or monthly subscription. Flexible cloud-connected licensing and automatic updates make it easy to manage NX use in your organization, reducing IT and maintenance expenses.
Global manufacturer relies on NX and Teamcenter to design wind turbines for leading energy and utilities companies around the world
See all Success Stories