Plano, Texas, 14 November 2017

Siemens’ Latest Version of NX Expands Toolset for Digitalizing the Machine Shop

  • Expanded software toolset integrates additive manufacturing, machining, robotics and quality inspection to digitalize part
  • Advanced automation capabilities connect end-to-end processes bringing machine shops greater efficiency and shorter time to job delivery
  • NX Machining Line Planner uses a digital twin of the complete machining line to optimize high-volume production for complex parts

The latest version of Siemens’ NX™ software unites the next generation of tools for additive manufacturing, computer numerical control (CNC) machining, robotics and quality inspection to enable the digitalization of part manufacturing within a single, integrated, end-to-end system. Advanced automation capabilities for computer-aided manufacturing (CAM), including robotic programming, adaptive milling, and tooling design, provide innovative, industry-specific technology to help deliver high-quality products to the market in less time. The new NX Machining Line Planner tool, combined with integrated NX CAM software for feature-based machining, provides new capabilities for industries with high-volume production of complicated parts, such as automotive and industrial machinery. The latest version of NX continues to support end-to-end solutions for additive manufacturing, helping manufacturers realize the goal of using 3D printing for industrial production.

Part manufacturers continue to face added pressures from changing market expectations, with customers who require improved accuracy and faster response times. In order to remain competitive, many part manufacturers look to digitalization, which connects all of the steps of part manufacturing planning and production with a single source of information, or a digital thread. Implementing a digital strategy can enable part manufacturers of all sizes to take greater advantage of automation, adopt 3D printing for production, and ultimately expand into new market opportunities and reduce time to delivery.

“In order to grow their businesses and expand into highly competitive markets like the aerospace and semiconductor industries, machine shops need to offer additive manufacturing combined with a highly automated process chain that digitally connects design, print preparation, NC and quality inspection programming to production,” said Christoph Hauck, managing director of New Technologies and New Markets, MBFZ toolcraft GmbH, an early adopter of Siemens’ additive manufacturing technology. “Siemens offers all of these capabilities in one complete and integrated system for part manufacturing. This allows us to link each step in our digital process chain, providing critical process control, associative data flow and traceability – which are important for our customers.”

New automation enhancements within the latest version of NX provide powerful ways to expand production efficiency and reduce cost. Robotic programming technology provides the ability to automate complete manufacturing cells, including programming robots to perform machining and pick-and-place operations. Adaptive milling and tube milling are new capabilities that provide innovative ways to automate CNC machine programming and accelerate cutting of complex parts. Adaptive milling is a high-speed cutting method that leverages automation within NX to reduce machining cycles by up to 60 percent while extending tool life. Tube milling streamlines the 5-axis programming process by eliminating preparation and minimizing inputs, utilizing advanced capabilities to create ideal tool paths and minimize errors in machining on the shop floor.

Mold and die manufacturers can now automatically and accurately determine tool production costs through seamless integration between NX and the Teamcenter® portfolio. Engineers can now use NX to automatically recognize features and parameters on the desired part, and provide pertinent information to Teamcenter, which can precisely calculate the tool cost. The newly integrated capabilities of Siemens’ product lifecycle management (PLM) software solutions can enable tool manufacturers to win more orders and increase profit margins through automated costing and accurate quotations.

New to this version, NX Machining Line Planner, combined with integrated NX CAM, enables the feature recognition, distribution, balancing, programming and simulation of operations over multiple setups and machines. Particularly helpful for industries with high-volume production of complicated parts with many features, NX Machining Line Planner uses a digital twin of the complete machining line and NX CAM feature-based machining technology to optimize the entire process. NX Machining Line Planner, combined with the power of the digital twin, offers a truly unique solution that enables automotive and machinery manufacturers to reduce planning time and increase overall production results.

The latest version also expands the new additive manufacturing solution in NX by including the new module, NX AM for HP Multi Jet Fusion, which is certified by HP and powered by Materialise, to prepare print jobs for HP Jet Fusion 4200 3D printers. The NX software module will allow customers to develop and manage parts in a single software environment for Multi Jet Fusion printing solutions, avoid costly and time-consuming data conversions and third-party tools, and improve their overall design-to-finished-part workflow efficiency. Additionally, Siemens develops applications for additive manufacturing process simulation in Simcenter 3D, a crucial tool to help manufacturers industrialize additive manufacturing by printing components the first-time-right. These simulation applications are an integral part within the Siemens’ end-to-end additive manufacturing solution.

“Transformative technologies like additive manufacturing and advanced robotics offer tremendous potential for manufacturers of all sizes to gain an advantage in today’s competitive market,” said Zvi Feuer, senior vice president of Manufacturing Engineering Software for Siemens PLM Software. “NX provides a fully integrated solution for part manufacturers to utilize these powerful technologies, creating the ability to improve overall business performance and helping to create a truly digital machine shop.”

For further information on NX for Manufacturing, please see https://community.plm.automation.siemens.com/t5/News-NX-Manufacturing/What-s-new-in-NX-12-for-Manufacturing/ba-p/440289.

Siemens PLM Software, a business unit of the Siemens Digital Factory Division, is a leading global provider of software solutions to drive the digital transformation of industry, creating new opportunities for manufacturers to realize innovation. With headquarters in Plano, Texas, and over 140,000 customers worldwide, Siemens PLM Software works with companies of all sizes to transform the way ideas come to life, the way products are realized, and the way products and assets in operation are used and understood. For more information on Siemens PLM Software products and services, visit www.siemens.com/plm.

Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 372,000 employees worldwide. Further information is available on the Internet at www.siemens.com/plm.

Note: Siemens and the Siemens logo are trademarks or registered trademarks of Siemens AG. NX and Teamcenter are trademarks or registered trademarks of Siemens Product Lifecycle Management Software Inc. or its subsidiaries in the United States and in other countries. All other trademarks, registered trademarks or service marks belong to their respective holders.

Follow us on Twitter at: www.twitter.com/siemens_press

Primary Contact

Siemens Digital Industries Software PR Team

press.software.sisw@siemens.com