Primary Contact
Larry
Toda
503.685.1664
larry_toda@mentor.com
WILSONVILLE, Ore., May 23, 2016 - Mentor Graphics Corporation (NASDAQ: MENT) today announced a new MicReD® Power Tester 600A product which tests electric and hybrid vehicle (EV/HEV) power electronics reliability during power cycling. The MicReD Power Tester 600A offering allows EV/HEV development and reliability engineers to test power electronics (such as insulated gate bipolar transistors – IGBTs, MOSFETs, transistors, and chargers) for mission-critical thermal reliability and lifecycle performance. Thermal reliability issues can result in EV/HEV automotive recalls, and the ever wider adoption of electric and hybrid cars has created a specific need for this solution. The Mentor Graphics® MicReD Power Tester 600A product also meets the industry’s need for power electronics thermal simulation and test, delivering unmatched accuracy and scalability.
Delta Electronics develops high-efficiency and high-density power module products. “We apply the Power Tester 1500A to gain insight into the lifetime performance and assure the reliability of the IGBT module,” said Andy Liao, section manager, Delta Electronics. “The Power Tester 600A could provide a scalable solution that would allow us to measure many discrete power devices or modules concurrently. This increased testing throughput would give us statistical failure data that we need in order to accurately predict the field lifetime of the products.”
Reliability, Accuracy and Scalability Solves EV/HEV Power Electronics Thermal Issues
Designers of today’s EV/HEVs are faced with significant mission-critical challenges: foremost among these is ensuring the thermal reliability of power electronics modules; detecting potential degradation of IGBTs caused by a range of standard drive cycles; and identifying the underlying damage root causes. Mentor’s MicReD Power Tester 600A solution provides accurate and reliable test results that scale to real-world requirements:
MicReD Power Tester 600A – Part of a Comprehensive Solution
Mentor Graphics is uniquely positioned as the only company that can provide a complete thermal software simulation and hardware testing solution specifically for the EV/HEV market. The MicReD Power Tester 600A product can be coupled with Mentor’s leading CFD simulation technologies. Mentor’s FloTHERM® and FloEFD™ 3D CFD software provide front-loading thermal simulation of power modules. When coupled with the Flowmaster® full vehicle thermo-fluid system-of-system 1D CFD modeling tool, this yields unparalleled levels of accuracy. This is done by MicReD’s T3Ster technology providing CFD input material properties for automated model calibration functionality to accurately simulate the real temperature response of an EV/HEV’s dynamic power input. This combination of technologies allows users to generate IGBT thermal lifetime failure estimations with the greatest accuracy possible.
“The MicReD Power Tester 600A is an extension of our total solution in automotive thermal engineering, and there is no other product like this for the EV/HEV market today,” stated Roland Feldhinkel, general manager of Mentor Graphics Mechanical Analysis Division. “We have leveraged our best-in-class products to deliver a comprehensive thermal simulation and hardware test solution that meets auto maker EV/HEV industry needs while supporting the rapid growth forecast for the market in the next few years.”
Product Availability
Mentor Graphics is now accepting orders for the MicReD Power Tester 600A with shipping scheduled for summer of 2016. For additional product information, please visit the company website: www.mentor.com/powertester-600a.
(Mentor Graphics, Mentor, FloTHERM, Flowmaster, and T3Ster are registered trademarks, and FloEFD is a trademark of Mentor Graphics Corporation. All other company or product names are the registered trademarks of their respective owners.)
Larry
Toda
503.685.1664
larry_toda@mentor.com