19 October 2016

Mentor Graphics Announces Availability of Qualified Calibre PERC Rule Decks for UMC 28nm Technology

Highlights: Mentor Graphics announces the availability of qualified Calibre® PERC™ reliability rule decks from UMC for their 28nm technology.

WILSONVILLE, Ore., October 19, 2016— Mentor Graphics Corporation (NASDAQ: MENT) today announced the availability of qualified Calibre® PERC™ reliability rule decks from United Microelectronics Corp. (UMC) for their 28nm technology.  Customers of UMC can now extend their use of Mentor-based flows to incorporate advanced electrical reliability analysis that evaluates a variety of electrostatic discharge (ESD) protection features.

“New design requirements such as ESD protection are essential for ensuring the long-term reliability of integrated circuits,” said T.H. Lin, director of the IP Development and Design Support Division at UMC. “By providing rule decks for Mentor’s Calibre PERC reliability platform to our customers, we ensure that they have the ability to analyze designs and confirm adequate protections are in place to prevent ESD failures once these chips enter the market.”  

The Calibre PERC reliability platform enables designers to analyze physical and electrical properties in tandem, enabling complex reliability checks. The Calibre PERC design kits available from UMC include coverage for electrostatic discharge protection, power clamp circuit verification, the verification of current density on an ESD path, and the verification of point-to-point (P2P) resistance on power/ground along an ESD path.  

"With the rapid growth in new IC applications for the automotive, industrial, and medical devices markets, extended reliability is becoming a necessity, not just a market differentiator,” said Carey Robertson, Calibre Design Solutions marketing director for circuit verification and reliability. “Companies such as UMC that take the necessary steps to ensure their customers’ designs achieve the new reliability standards will be well-positioned to succeed in those markets.” 

The challenge of IC verification in today’s complex designs is enormous. Automated reliability verification tools such as the Calibre PERC reliability platform help designers ensure their products can not only be manufactured, but will perform as designed throughout their intended lifecycle. By adding Calibre PERC design kits to their portfolio, UMC is providing its customers with additional capabilities to deliver reliability-proven designs to the marketplace.

(Mentor Graphics, Mentor, and Calibre are registered trademarks and PERC is a trademark of Mentor Graphics Corporation. All other company or product names are the registered trademarks or trademarks of their respective owners.)

Primary Contact

Suzanne Graham
503.685.7789
suzanne_graham@mentor.com

Have Questions?