Noise, Vibration & Dynamics Performance Optimization for HVAC

HVAC systems are in people’s homes and are where people work, and so we want these systems to be as quiet as possible.  Additionally, too much vibration can lead to excessive wear and reliability issues of the system.  Delivering a quiet system that ends customers want can be a challenge if you don’t truly understand the performance of your furnace, air conditioner or heat pump and the source of the noise and vibration.

Siemens Digital Industries Software offers a comprehensive set of advanced vibration and acoustic simulation and testing solutions that can help you predict the dynamic and acoustic performance of your HVAC system earlier in the development process, as well as determine the source and transfer path of noise in systems that are already installed in buildings.

HVAC systems are in people’s homes and are where people work, and so we want these systems to be as quiet as possible.  Additionally, too much vibration can lead to excessive wear and reliability issues of the system.  Delivering a quiet system that ends customers want can be a challenge if you don’t truly understand the performance of your furnace, air conditioner or heat pump and the source of the noise and vibration.

Siemens Digital Industries Software offers a comprehensive set of advanced vibration and acoustic simulation and testing solutions that can help you predict the dynamic and acoustic performance of your HVAC system earlier in the development process, as well as determine the source and transfer path of noise in systems that are already installed in buildings.

Learn More

Noise and vibration are critical performance aspects of HVAC systems.  Too much of either can have a negative impact on the quality of life and comfort for those living and working nearby. Uncontrolled vibration can also directly impact the reliability and longevity of the entire system. To deal with noise and vibration problems, HVAC engineering departments require a very comprehensive set of simulation and testing solutions. These should be capable of handling target setting, product design, refinement, final prototype validation, certification, troubleshooting and more.

Siemens Digital Industries Software simulation and testing solutions can help you spot resonances and noise sources, even from the most unexpected sources. Our portfolio of dedicated noise and vibration solutions includes 3D simulation tools that can be used during early development to predict fan dynamics, vibration and interior and exterior acoustics.  Additionally, Siemens offers the hardware and noise testing expertise for noise, which can be deployed on physical prototypes as well as for correcting issues with existing HVAC installations.

Solution capabilities

Explore the key areas of this solution.

Acoustic Testing

Design innovative products with a compelling acoustic signature that conform to the latest international standard and adjust to your project requirements.

Acoustics Simulation

Design innovative products with a compelling acoustic signature that conform to the latest international standard and adjust to your project requirements.

Dynamic Environmental Testing

Select a comprehensive solution for dynamic environmental testing that ranges from routine vibration qualification tools to effective, high-speed multi-channel closed-loop shaker control system with parallel data acquisition and powerful analysis capabilities.

Engineering & Consulting

Accelerate product development and solve the toughest problems with scalable help from engineering and consulting services.

Hardware & Data Acquisition

Streamline your purchase, testing and maintenance processes by selecting hardware from a partner that supplies end-to-end solutions for your multi-physics testing requirements, from sensors and exciters to comprehensive data acquisition.

Motion Simulation

Calculate the reaction forces, torques, velocities, acceleration and more for mechanical systems. This allows you to convert CAD geometry and assembly constraints into an accurate motion model.

Rotating Machinery Testing

Optimize performance of rotating machinery, by acquiring and analyzing impact of speed, torque and control strategy on sound quality, (torsional) vibrations, and energy efficiency.

Structural Dynamics Testing

Maximize your testing efficiency, when performing impact testing on small structures, running large-scale campaigns with hundreds of measurement channels, or validating 3D finite element models with experimental data.

Interested in [[global-preference-center-interest-placeholder]]?

Subscribe to [[global-preference-center-interest-placeholder]] updates

Oops

We're very sorry, but we weren't able to capture your submission. Please try again.

Thanks for signing up! First time subscribing? Be sure to check your email to confirm your subscription.

Field is required A valid email address is required
Field is required Invalid value or too long