Mercedes-Benz AG and Daimler Truck AG will start to use NX 2212.3001.257.201 on 18-March-2024.
Download instructions:
The files necessary for installing this hotfix are packaged in the zip files named SiemensNX-2212.3001.257.201_wntx64_MSI.zip and SiemensNX-2212.3001.257.201_wntx64_MSP.zip which are available for downloading from the Siemens Digital Industries Software Support Center using the following steps.
Notes: A valid WebKey account is required
- In your browser address window enter the URL:
- https://support.sw.siemens.com/en-US/product/209349590/download/PL20230216568348020
- User: (your email address)
- Password: (your WebKey password)
- Download: SiemensNX-2212.3001.257.201_wntx64_MSI.zip or SiemensNX-2212.3001.257.201_wntx64_MSP.zip
The MSI installer can be used to upgrade but is ideally suited for new installs. The MSP installer will only upgrade to a previously installed NX 2212.3001. Please see Siemens_HotFix_Install.pdf for more detailed instructions.
After downloading the zip file, you can use certutil to verify that the SHA-512 hash value matches between the zip file and the hash listed in the full or MSP SHA512 zip file.
If the link above does not open or shows no content:
Open a support case and ask to add the hotfix to your account. Because logging in is already done, click in the Support Center on “Support Cases > Open a new Support Case”