Innovation and collaborative, synchronized program management for new programs
The power of additive manufacturing is the ability to generate new designs that could not be developed by traditional manufacturing processes. This capability allows us to create organic shapes that normally are impossible to manufacture. Additive manufacturing permits exploration of multiple design alternatives to find optimal designs quickly. Our solutions for additive manufacturing enable you to reimagine products, retool manufacturing and rethink business models.
The power of additive manufacturing is the ability to generate new designs that could not be developed by traditional manufacturing processes. This capability allows us to create organic shapes that normally are impossible to manufacture. Additive manufacturing permits exploration of multiple design alternatives to find optimal designs quickly. Our solutions for additive manufacturing enable you to reimagine products, retool manufacturing and rethink business models.
A convergence of technologies is opening up new possibilities in design. Designers can designate the important functions and parameters of a design, and produce shapes inspired by nature and optimize for material use, strength, and other factors. It’s also much easier to explore multiple design alternatives to find the one that works best and create radical new designs. Additive Manufacturing allows us to create prototypes to validate these designs for performance.
However, techniques such as directed energy deposition, fused deposition modeling, laser material fusion, and agent jetting or inkjet technology are moving additive manufacturing beyond prototyping and into large volume production. With our solutions, you can scale additive manufacturing from prototypes to mass production, all in the same system with change management and requirements tracking.
These solutions enable companies to take advantage of new manufacturing methods to produce innovative designs, create lightweight parts that weren’t possible in the past, validate designs before production and scale up from prototype to mass production in a single system.
Additive manufacturing is more than just 3D printing of parts and prototyping. It can be a launch pad for you to re-image products, reinvent manufacturing and rethink business.
Explore the key areas of this solution.
Securely manage the data encompassing the entire additive manufacturing process including the printing process itself as well as material handling and manufacturing operations.
Adopt a compromise-free approach to physics modeling using best-in-class simulation tool
Additive manufacturing is changing the way products are designed as well as how they are manufactured, by enabling optimized designs that were previously impossible or too expensive to make.
Complete visibility, control and optimization of production and processes across the enterprise
CAD to CAE easy integration with Simcenter
Webinar on optimizing parts in multiple ways for additive manufacturing
Learn more about the full potential of additive manufacturing 3d printing, and how to robust process that integrates additive design, engineering, ...
Additive Manufacturing (AM) offers tremendous opportunities for innovations in manufacturing operations. In order to realize the full potential of ...