Innovation and collaborative, synchronized program management for new programs
It is necessary to optimize electrical and electronic system architectures against targets such as cost, weight, and network bandwidth. As architectural decisions have significant long term product impacts, being able to rapidly design, iterate, and optimize as early as possible in the development process leads to significant benefits all through the subsequent stages of bringing complex products to market.
It is necessary to optimize electrical and electronic system architectures against targets such as cost, weight, and network bandwidth. As architectural decisions have significant long term product impacts, being able to rapidly design, iterate, and optimize as early as possible in the development process leads to significant benefits all through the subsequent stages of bringing complex products to market.
It is vital to be able to automatically or manually allocate functions and signals to resources and carriers using rules-driven logic, incorporating constraints. This has been coupled with the ability to optimize function allocations to balance resource utilization, cost, and mass across the entire platform and have the ability to perform fast 'trade studies' to analyze allocations and rapidly re-assess the resource balance resulting from each change. All of this platform content can be verified using customizable design rule checks.
Engineers need to capture and consolidate function characteristics and connectivity, so they can develop optimized implementations within platforms. Software, hardware, networks, and electrical functions can be managed together in a lightweight environment that allows these disciplines to collaborate easily.
It is important to be able to generate implementation details to feed downstream processes designing electrical hardware, software, networks, and Electrical Distribution System (EDS). Engineers also need to extract logical and physical content, which is synthesized as correct-by-construction from the platform designs, controlled by corporate defined rules and constraints.
Prepare to make the most of your investment
The shift to a software-defined vehicle is accelerating. But there are challenges: Software complexity growth has outpaced predictions, safety and ...
Trendy napříč odvětvími jsou hned v několika oborech výzvou pro tradiční postupy. Elektrifikace je na vzestupu, výrobky ve všech odvětvích jsou stá...
Vehicles in all sectors are growing in complexity as OEMs develop sophisticated platforms with increasing levels of automation and connectivity, dr...