Tools


Contact
Close Contact Layer

Contact Siemens PLM Software


5800 Granite Parkway
Suite 600
Plano TX USA 75024

(v) +1 800 498 5351


Case Study

Company-wide transition to 3D modeling

Alexin Joint Stock (Tyazhpromarmatura)

Russia’s largest valve supplier standardized (design automation) on Solid Edge

Valves for harsh environments

Alexin Joint Stock Company, Heavy Industrial Valves (known as Tyazhpromarmatura in Russian) was established in 1778. The company designs and manufactures valves and gates for gas, oil, chemical and power industries. Today Tyazhpromarmatura is the largest valve maker in Russia and the Commonwealth of Independent States, which is composed of 11 former Soviet republics. The company’s major clients are the largest oil and gas extracting and transporting companies: Gazprom, Transneft, Lukoil, Tatneft and others.

The company’s primary products are slide and wedge gate valves, and ball valves. These products are used in harsh conditions, such as under strong oil and gas pressure, in explosive atmospheres, in polar climates and so on, where quality requirements are very high.

Tyazhpromarmatura’s diversification policy is aimed at developing advanced products such as valves for nuclear and thermoelectric power plants, as well as ball valves for gas and oil that contains abrasive components. For example, testing has been successfully completed for a 300 mm (approx. one foot) gate valve withstanding pressures of PN 11MPa and temperatures of more than 300 degrees (C) to be used with two different types of Russian nuclear reactors. Currently the valve is in production for nuclear power stations at Voronezh, Saint-Petersburg and Rostov regions. Annual sales exceed 50,000 units.

A new CAD solution for design automation

At the beginning of 2007, Tyazhpromarmatura decided to automate its product development process. The primary goals of the project were saving design and production planning time, and enhancing the quality of products and management processes. The first stage of the project was the selection of a software solution. A working group of leading engineering experts was established under the supervision of Tyazhpromarmatura’s IT department. “The project’s basic goals were to establish a single design approach across the entire company, to transition to a single data format and to improve the quality of design documentation,” says Mikhail Gusev, head of the company’s IT department. “We decided to start by choosing a CAD system.”

For half a year the company’s experts analyzed the CAD market. Four well-known CAD systems were selected for further consideration, two being Russian and two being foreign, including the Solid Edge® CAD program from Siemens PLM Software. After a thorough analysis, they decided to purchase Solid Edge.

“While selecting the system, we used cost-to-quality analysis and considered that the final output of the designer’s work is a drawing, so the functionality for drawing generation and standards-compliant annotation was very important,” says Gusev. “We also needed a scalable solution that would allow us to later switch to a complete digital mockup and provide integration with CAM systems.” Among the proposed systems, only Solid Edge met all the requirements and successfully passed a test for building complex curved blends, which are common in the company’s products. An additional benefit was Solid Edge’s integration with the entire set of Siemens PLM Software products.

Fast transition

In March, 2007 Tyazhpromarmatura started a Solid Edge implementation project. The objective was a deployment of Solid Edge 2D across the company as the standard CAD system and a step-by-step implementation of Solid Edge 3D.

The implementation team included two designers and one IT engineer. The designers received training from Siemens PLM Software, gaining experience in Solid Edge’s installation, customization and usage. They then developed a standard Solid Edge drafting process that includes a compliance verification procedure applied to the digital documentation. It also includes the rules of using templates and customization tools. Thanks to its great flexibility, Solid Edge was easily configured to meet the company’s workflows and standards.

After that, specialists from Siemens PLM Software started teaching 2D modeling to the other designers and manufacturing engineers. Training in 3D modeling was also performed by Siemens. The hardware was tested and updated while the training was going on so that afterwards, employees could start working immediately.

The project’s outcome was more than 80 Solid Edge workstations, training, documentation, manuals and finally, product development with Solid Edge. The transition to Solid Edge took just three months. This was possible thanks to the experience of the company’s specialists as well as the capabilities of Siemens PLM Software’s solution, such as compatibility with many different data formats, easy learning, compliance with national standards, flexible customization, floating licenses and the technical support and training provided by the supplier.

Promising early results

Currently Solid Edge is the only CAD system in use across the company. It is used in the design and production planning departments, at the equipment maintenance and power supply services, and on the shop floor. As Gusev notes, “After the transition to Solid Edge, we have a single data format company-wide.”

Even more important is that the transition to 3D modeling has begun. “We need 3D models to be able to evaluate the assembly process, and for finite element analysis, NC programming and mold design,” says Gusev. Besides that, the designers at Tyazhpromarmatura have observed that creating 3D models in Solid Edge and consequent generation of drawing views and sections saves a lot of time compared to manual drafting. And photorealistic images and animations created with Solid Edge help promote complex customized products.

Thanks to the successful experience with Solid Edge, Tyazhpromarmatura may be implementing other Siemens PLM Software’s solutions in the future. The company is now considering the Teamcenter® solution as its PLM system and NX™ CAM software as its primary CAM system. The excellent functionality of fully integrated solutions from Siemens PLM Software, their flexibility, easy learning curve and attractive cost of ownership have made the software choice for the leading Russian valve manufacturer.

Close share layer

Share this page

Share this page through any of the following channels.

Bookmarking Sites

Communities

News

Blogs & Microblogs