Tools


Contact
Close Contact Layer

Contact Siemens PLM Software


5800 Granite Parkway
Suite 600
Plano TX USA 75024

(v) +1 800 498 5351


Case Study

Aerospace electronic systems pioneer uses Siemens PLM Software technology to reduce load cases by 90 percent

Hispano-Suiza

LMS solutions help Hispano-Suiza improve the reliability of analysis results, enhance the performance of the RAT and bolster its credibility and communication with Embraer

Finding issues

Hispano-Suiza, a Safran Group company, is a pioneer in the design, development and production of electronic power controllers for airborne applications. In 2012, the company celebrated the delivery of its 30,000th power transmission.

Hispano-Suiza was contracted by Brazilian aerospace manufacturer Embraer to do all the electrical distribution work, which includes the ram air turbine (RAT), for the Embraer KC-390, a medium-size, twinengine, jet-powered military transport. The KC-390 is able to perform aerial refueling, transport cargo and troops and receive fuel in-flight. It will be the heaviest aircraft that the company has ever produced, and will be able to transport up to 23 tons of cargo, including wheeled armored vehicles.

The RAT is a small turbine that is connected to a hydraulic pump or electrical generator that is used as an emergency power source capable of delivering enough electricity to run flight control systems. The RAT is able to generate power from the airstream due to the speed of the aircraft. RATs are common in military aircraft, which must be capable of surviving a sudden and complete loss of power.

The RAT must fit in a very confined space and the occurring loads must stay below the defined limits. By using LMS Virtual.Lab™ Motion software and LMS Imagine.Lab Amesim™ software from Siemens PLM Software, Hispano-Suiza was able to fulfill both requirements.

“If we didn’t have LMS Virtual.Lab and LMS Imagine.Lab during the design phase, we wouldn’t have discovered an inadvertent opening in the RAT in flight,” says Julien Guiraud, the Hispano-Suiza mechanics manager for the RAT KC 390 calculation and aircraft integration project. “They helped us to find such problems, and to discover some physics problems during the deployment that we absolutely didn’t expect.”

Improving physics insight

Hispano-Suiza recognized it needed a new design process that would provide improved physical insight of the model; enhance the validation process when exchanging information with Embraer and the different subcomponent suppliers (for example, on damping of the system) and shorten the simulation and model validation phase.

By using LMS Imagine.Lab, Hispano-Suiza was able to cross-check the system damping analysis performed by the suppliers on the design of the hydraulic system.

“When you deploy the RAT, you need to slow it down at very high air speed,” says Guiraud. ”To avoid any failure, we created a hydraulic LMS Imagine.Lab model to work in parallel with our supplier; first to validate the supplier result and, second, to quickly answer any questions from Embraer knowing that if you change parameters like compressibility of the fluid or temperature variation, the damping performance during deployment will be increased.”

In addition to the damping characteristics, the Hispano-Suiza engineers also gained a lot of insight into the kinematic and dynamic performance of the RAT, the loads and the stresses.

Reducing load cases

The KC-390 engagement provided a number of significant challenges for Hispano- Suiza. If Hispano-Suiza wanted to maintain its status as a trusted partner of Embraer, it needed to design the RAT correctly the first time even though this was the company’s first attempt at developing this piece of equipment. The company also needed to provide Embraer with loads, performance and stress results for a variety of load cases to make sure it met Embraer’s specifications.

This presented a number of potential issues, including running and analyzing an enormous number of loads, the risk of errors and providing suppliers with the relevant load cases. It also meant performing kinematics and dynamics simulations, which required the ability to optimize the model to fit boundary conditions.

“Thanks to the use of a multi-body dynamic model, which includes the flexibility of all the components, we discovered that nonlinear problems were created,” says Guiraud. “As a result, we used the LMS Virtual.Lab Motion to check the stress in specific cases that we wouldn’t have discovered using other analysis packages.”

Realizing clear benefits

There were many challenges to implementing new processes and tools, including finding parts that were too flexible and could have led to the loss of door pretension and dramatic failures during the first flight; adjusting kinematic processes according to peaks of loads during the deployment; and developing a better understanding of the influence of parameters on the design and integration in the aircraft.

Not only did Hispano-Suiza find potential problems, but by using LMS Virtual.Lab Motion and LMS Imagine.Lab Amesim, it also reduced the number of load cases to be analyzed by 90 percent – from 500 to 50 – and cut the time it took to conduct the load cases by 30 to 40 percent. The LMS solutions also helped Hispano-Suiza improve the reliability of the analysis results, enhance the performance of the RAT and bolster its credibility and communication with Embraer.

Demonstrating reliability

By gaining a deeper physical insight into the KC-390 program, Hispano-Suiza is now in a better position to demonstrate the reliability of its methods and models, giving it a competitive advantage. Hispano- Suiza plans to use optimization tools with the model to investigate computation fluid dynamics (CFD) links in conjunction with Siemens PLM Software tools and fatigue simulation in order to have the full loop of loads and designs in one model.

Embraer’s experience with LMS Virtual.Lab Motion and the team that supports them has enhanced the confidence that it has in Hispano-Suiza’s expertise, and makes it possible that Siemens PLM Software will be included in future Embraer programs. Moreover, Hispano-Suiza has confidence in the LMS Virtual.Lab Motion solution and the Siemens PLM Software team, making it likely they will be using the software in future programs.

Close share layer

Share this page

Share this page through any of the following channels.

Bookmarking Sites

Communities

News

Blogs & Microblogs