JT2Go now supports optional Asian fonts for product manufacturing information (PMI).
The file below contains the stroke information needed to draw Asian characters (JaPCK, JaEUC, ZhGBK, KO, and ZhBIG5).
This is useful if (a) the .jt has PMI that uses Asian characters and (b) the machine is in the same locale settings as the PMI.
If we cannot draw the authored character (either because of the locale or VPPMIFonts.bin is missing) a # character will be drawn instead.
Download the zip file below and extract into the JT2Go loadpoint/etc (e.g., C:\Program Files\Siemens\JT2Go\etc). Once you have extracted the VPPMIFont.bin file into that folder you can discard the zip file.
上海市长宁路1018号龙之梦大厦13楼
上海市 200042
中国
(v): +86 21 2208 6688
Share this page through any of the following channels.