LANDMARK TECHNOLOGY CORPORATION does business in two fields; the 3D graphics and the plasma process. In the 3D Graphics area, LANDMARK sells and supports the 3D Viewer "LANDMARK VIEW" and the 3D Real Time Collaboration System "GlobalVision". LANDMARK was a collaboration partner with UGS from the SDRC era and has experience in dealing with the IDI format for manipulating 3D dimension annotation. Now LANDMARK can work with the JT format so that customers using IDI will have a smooth transition to JT.
164 87 KISTA
Besöksadress: Kronborgsgränd 7a
Sverige
(tel): +46 8 506 990 00
Share this page through any of the following channels.