Teamcenter Express Version 5 builds on its proven delivery of a preconfigured cPDM environment for small- and medium sized manufacturing organizations with an updated user interface, new cost analysis tools for products and projects, enhanced integration with Microsoft Office and expanded project scheduling capabilities. These new capabilities can increase your productivity and your ability to complete design-through-manufacturing projects on time and on budget
Teamcenter Express Version 5 is a configuration of the industry’s most widely implemented PLM solution, Teamcenter, delivering best-in-class scalability and performance, and takes advantage of the latest developments in Teamcenter 8
“The release of Teamcenter Express Version 5 on the latest Teamcenter platform adds a well-rounded set of new productivity improvements to this comprehensive cPDm solution for SMBs” said Peter A. Bilello, Vice President, CIMdata. “The enhancements in Version 5 such as the comprehensive integration with Microsoft Office and the new cost analysis tools for both products and projects should further enable small- and mid-size manufacturing organizations to deliver their design projects to manufacturing on time and on budget while improving their own cost management.”
Siemens PLM Software adds significant new capabilities to Teamcenter Express Version 5 that further establishes Teamcenter Express as the leader in providing a preconfigured cPDM environment that focuses on managing everyday tasks and processes for design-through-manufacturing for small and mid-sized organizations. The updated user interface, new cost analysis tools for products and projects, enhanced integration with Microsoft Office and expanded project scheduling capabilities increase productivity from the users’ desktop through to manufacturing
Teamcenter Express users benefit from extensive updates to the user interface that speed the user’s learning curve and improve productivity and consistency in completing everyday tasks:
An enhanced reporting tool enables product costs to be calculated, stored and analyzed throughout the product lifecycle. This enables better control of costs from concept design through to release to manufacturing leading to better control of costs and increased profitability. In addition to cost analysis, reports can also be used to analyze weight and other user defined attributes.
Version 5 adds an improved user interface and expanded capabilities for integration with Microsoft Office. Users of Microsoft Office 2007 Word, Excel and Powerpoint can easily browse and search the Teamcenter Express database while working in these applications, can add new documents to the single source of data and review and approve PDM workflow tasks that have been assigned to them. Users of Microsoft Outlook can also see all the PDM workflow tasks that are assigned to them, and review and signoff on these tasks and the associated documents.
Version 5 includes several enhancements in the optional project management module that is available with Teamcenter Express. These include the ability to create links between projects so you can create a master project with sub-projects, users can also view multiple project schedules in a single window, enabling improved resource allocation and early identification of potential bottlenecks. Project cost rollups are also now available enabling calculation and analysis of project costs throughout the project lifecycle.
Teamcenter Express Version 5 is built on and delivers complete scalability to the unified architecture of Teamcenter 8. Teamcenter is the proven global leader in PLM with over 5 million licenses and delivers proven scalability to Teamcenter Express users in terms of complexity of data being managed, number of users accessing the database, and scope of processes that are managed.
Decrease Text Size Enlarge Text Size Text Size
Express Version 5 fact sheet provides additional details of the new features and options in Teamcenter.
Estas demonstrações disponibilizam uma visão geral de alguns dos novos e principais recursos do Teamcenter Express Versão 5:
Press Release
Teamcenter Express Version 5
Av. Goiás, 1320 - São Caetano do Sul
Brasil, SP -
09121-300
(t): +55 (11) 4224-7155
Share this page through any of the following channels.